FAQs durchsuchen



What materials are used in the main structure and acoustic foam lining of the NetShelter CX?
The NetShelter CX also uses a combination of Medium Density Fibre Board (MDF) and High Pressure Laminate ( HPL ) on its top ...
Technical Explanation as to why the batteries individual inside the SYBT5 Module should not be replaced
There is a circuit board inside the module that is calibrated to the individual batteries. This provides the sophisticated battery management that the LX offers.
Humidity Issues in IT Data Centers
Fluctuations in humidity: * Large fluctuations in humidity can cause circuit boards to expand and contract, damaging circuitry
Universal Transfer Switch (UTS) – FAQ
If the UTS circuit board were to fail, what is the expected behavior? Will my circuits have power?
Back-UPS is detected as an ""Unknown Device"" in Device Manger
Towards the bottom , you should ... will see, XXX ""Universal Host Controller"" and ""USB Root Hub"" ...
How do I reset the communication card of a SmartCell XR?
The SmartCell XR onboard microprocessor will turn itself off (sleep mode) after approximately 30 seconds if the communications cable is removed from the "BATT COMM OUT" jack. This is to prevent the board from discharging the batteries, down to dangerous levels, during shipping/storage. To successfully reset the communications module you need to wait for the board to go to sleep.
High Supply Temp Shutdown Installation on a NetworkAIR FM
This board below is called the Programmable Customer Input/Output Module (PCIOM). The PCIOM can be found in the User Interface Box, which is located near the bottom on the left of the FM. See screen shot below.


Ergebnisse 1 - 10 von 51

Nicht gefunden, was Sie suchen?

Wenden Sie sich an unser Kundenteam, um Informationen zum technischen Support, Unterstützung bei Beschwerden und vieles mehr zu erhalten.