Technische FAQs

Fragen Sie uns

Die Ergebnisse filtern

    Is COO, HTTS or ECCN information available for NetShelter CX cabinets and accessories?
    ar4000mv12u NetShelter CX Mini 12U Vertical Mounting Rail Kit
    Where is the serial number located on the NetShelter CX or CX Mini?
    Issue: A customer needs to find the serial number on the NetShelter CX or CX Mini .
    Can equipment be installed on the floor of a NetShelter CX or CX Mini?
    Issue: Customers may ask if it's OK to install equipment on the floor of a NetShelter CX or CX Mini .
    Are the NetShelter CX and CX Mini delivered fully assembled?
    The NetShelter CX Mini arrives on its castors with the brush strip attached to the underside, on a pallet, and the keys inside ...
    What is the Thermal Capacity of the NetShelter CX Mini and CX2?
    Resolution: ar4000mv NetShelter CX Mini = 800w
    What is the rackmount depth within the NetShelter CX or CX Mini?
    NetShelter CX Mini has an available equipment depth of 700mm/27.5” in standard format.
    Is the PDU removable that's included inside the NetShelter CX ar4000mv?
    Issue: A customer wants to replace the PDU in a NetShelter CX Mini .
    Can the NetShelter CX be locked?
    The CX Mini ar4000mv also has a key lock securing the rear access panel.
    How often should the NetShelter CX dust filters be cleaned?
    NetShelter CX owners need to know how often to clean the dust filters. ... NetShelter CX ... In a normal office environment the dust filter should be cleaned every 12 weeks. ... In those cases we recommend customers buy a spare set of dust filters, to always have a clean set on hand.
    Ergebnisse 1 - 10 von 77