Technische FAQs

Fragen Sie uns

Die Ergebnisse filtern

    What materials are used in the main structure and acoustic foam lining of the NetShelter CX?
    The NetShelter CX also uses a combination of Medium Density Fibre Board ... (HPL) on its top and MDF on its plinth base .
    Is there a list of NetShelter CX spare parts and accessories available, with photos?
    cx , side, fan, power supply, hinge, fan ... adapter, cx2, mini, key, keys, psu, plinth
    Where do PDUs mount in the NetShelter CX?
    For a list of APC 0U PDUs that are compatible with all NetShelter cabinets please see Knowledge Base document FA158651.
    Are NetShelter SX, SV, CX or VX cabinets NEMA rated?
    The word "enclosure" is to be used to describe NEMA rated products. For more information please see Knowledge Base document FA225841.
    acdc1010 Hot Aisle Containment Rack Expansion Bundle Kit Installation (Manual)
    ... Rack Expansion Bundle Kit Installation (Manual ... ... Rack Expansion Bundle Kit is a complete ... ... Rack Expansion Bundle Kit is a complete ... ... Rack Expansion Bundle Kit . IF you plan to install a Rack Expansion Bundle Kit next to a PDU or UPS, then a PSX/PDU side panel (acdc1008, not included) must be installed on the PDU or UPS. ... The ceiling panels are configured in two different widths based on the size of the enclosures they span.. ... 3. Attach the plinth blocks to the enclosures, using four M8 × 25-mm screws
    Does APC offer a side airflow duct kit for the Cisco Nexus 7009, 7000 9-slot switch?
    ... .com/products/resource/include/techspec_index.cfm? base _sku=AR7725
    Is there a kit available to convert from a NetShelter SX cabinet to a NetShelter SX Networking cabinet?
    For a complete overview of the differences please see Knowledge Base article FA158652.
    Using Symmetra RM outside of a Rack (Symmetra RM Floor Mounting Kit)
    ... .com/products/resource/include/techspec_index.cfm? base _sku=SYOPT1&tab=models
    What is the rackmount depth within the NetShelter CX or CX Mini?
    With the optional accessory 12U Rack Kit for Mini (ar4000mv12u) installed there is an equipment depth of 600mm/23.6” ...
    Ergebnisse 1 - 10 von 63