Technische FAQs

Fragen Sie uns

Die Ergebnisse filtern

    Which keys are used with NetShelter cabinets and EcoAisle, and how customers can obtain them.
    Please use Part 0H-0292-SE as the replacement keys for all NetShelter CX door locks.
    Is the PDU removable that's included inside the NetShelter CX ar4000mv?
    Issue: A customer wants to replace the PDU in a NetShelter CX Mini.
    Schneider Electric Rack LCD products and perceived "Image Burn In" / Dead Pixel Policy
    ... "image persistence." Leaving the screen on 24 /7 is not considered proper operation and will void any warranty replacement terms.
    On the replacement NetShelter CX fan tray the center pin of the DC connector has a larger o.d.
    Issue: Will the original power supply fit onto the DC connector on the replacement fan tray?
    Where do PDUs mount in the NetShelter CX?
    The NetShelter CX includes a 14-15 outlet PDU. Some customers may want to replace it with a larger PDU.
    What can cause the laminate on a NetShelter CX to peel and how can it be fixed?
    Replace entire panel or re-apply using contact adhesive and brush. Recommended contact adhesive - EVO-Stick 528 or equivalent.
    NetShelter CX Air Filters are Difficult to Install.
    If you have one of the affected units we can supply a replacement joining plate that's user replaceable.
    What should I do if all or some of the fans in a NetShelter CX fail or are noisy?
    Single fan failure Possible cause - Damaged fan frame, failed bearing etc. Field Solution - Replace fan tray.
    Ergebnisse 1 - 10 von 60