Technische FAQs

Fragen Sie uns

Die Ergebnisse filtern

    How does a dirty air / dust filter effect the airflow and influence thermal capacity of a NetShelter CX cabinet?
    When a NetShelter CX is fitted with a set of dust filters it is expected that the airflow will be reduced by 3%.
    Can the NetShelter CX fans be turned on/off, or fan speed raised/lowered, remotely?
    A temperature sensor can also be used to set thresholds for alarms, or to turn outlets on/off.
    How often should the NetShelter CX dust filters be cleaned?
    In those cases we recommend customers buy a spare set of dust filters, to always have a clean set on hand.
    On the replacement NetShelter CX fan tray the center pin of the DC connector has a larger o.d.
    At the low speed setting the fan operates as the original fan unit did.
    Which keys are used with NetShelter cabinets and EcoAisle, and how customers can obtain them.
    NetShelter CX : ... Please use Part 0H-0292-SE as the replacement keys for all NetShelter CX door locks. This is a set of two (2) keys.
    Video: How to set up a Back-UPS Pro
    Product Line: Back-UPS PRO, BX/BR "G ". Environment:
    Why are the Dell ReadyRails II loose?
    NetShelter SX, VX, SV, CX ... It's also possible that the Dell ReadyRails is not set deep enough.
    Video: How to set up a Back-UPS ES G Series UPS
    Product Line: Back-UPS ES "G" Environment:
    Can the NetShelter CX be locked?
    Issue: The NetShelter CX needs to be locked
    Where can a NetShelter CX be deployed?
    Issue: Where can the NetShelter CX be deployed?
    Ergebnisse 1 - 10 von 71