FAQs durchsuchen



Matrix-UPS run time theory
... method the Matrix UPS calculates its estimated ... Matrix UPS ... on the Matrix UPS calculates the " ... " based on five variables: 1 . Age of ... 5 . Percentage of ... applied to the UPS . ... time the voltage levels off for a ... ... To allow the UPS to predict when ... ... curve, the UPS will be able ... ... at 40 volts DC the batteries are ... If the UPS load is too ... that when the UPS is on- ... When the UPS is first installed with a ... ... Hex) the UPS might begin a ... ... KBase document titled "Requirements for Matrix UPS " ...
How do I properly install/uninstall my SmartSlot accessory card into my UPS?
... into my APC UPS ? APC UPS Models - Single and Three Phase including Smart- UPS and Symmetra models Device UPS Management accessories including ... UPS Network Management Card 1 and 2 Interface Expander 1 /2 ... card while the UPS unit is in ... The first six characters should ... ... depending on your UPS type. Smart- UPS (SU, ... ... connected to the UPS Disconnect the UPS from its AC ... ... to turn the UPS off. ... button for approximately five seconds to turn off the DC (battery) ... ... then plug the UPS back in and ...
Video: Troubleshooting no communication between UPS and PowerChute Business Edition
... No Communication with UPS Troubleshooting Windows Serial Communications ... for Smart- UPS models SU, ... ... the "Checking UPS Communications on Windows ... ... For Smart- UPS models SMT, ...
Video: How do I configure APC Network Management Card network settings?
... Environmental Monitoring Unit 1 (AP9312TH) ... Network Management Card 1 (NMC1) ... ... Network Management Card 1 include (but ... ... , Smart- UPS Online (SRT ... ... Network Management Card 1 : ... Network Management Card 1 (AP9617, ... Network Management Card 1 (such as ... ... Network Management Card 1 based devices are ... ... device, select one of the available ... Smart- UPS front panel LCD ... Configuration Option 1 - Device IP ... ... , the APC UPS service must be ... ... with an APC UPS or accessory. ... Connect to the UPS /device serial ... Most UPS devices with a ...
Video: How to Start your Silcon UPS
How to Start your Silcon UPS ... The first step is to return utility power to the ups by turning the Q 1 switch on. ... “Stop Charge DC Capacitors: Yes” ... Start Charge DC Capacitors: Yes” ... UPS is now started . To take the UPS out of Maintenance Bypass do the following. Start by putting the ups into Static Bypass by pressing the # key ... The UPS is now out of Maintenance Bypass
SRT 8 or 10kva reports Error P.11 or DC Bus Soft Start or event codes 124/125
The UPS reports P.11 or DC Bus Soft Start - event 124/125 ... If the problem persists, Brain dead the UPS . If the alarm reoccurs, perform a UPS Firmware upgrade to the latest 04.7 revision that addressed these issues. ... Release Notes ( UPS 04.7): ... 1 . Improved system performance of transitions between Online and Bypass operation modes. ... 3. Improved system behaviour to eliminate false detection of DC bus under voltage alarm under certain conditions. 4. Improved system handling for certain AC input conditions during system start -up.
Where can I get support for APC and MGE Products?
... 6 0034- 1 0034-100 ... 2M- 1 E 0035nd-3M- 1 E 0039- ... ... 2M- 1 E 0088nd-3M- 1 E 0100- ... 2M- 1 E 0226- ... 3 0377- 1 M 0377- ... ... 2M- 1 E 0719- ... 7 0859- 1 0859-10 ... ... 15M 12000- 1 M 12000- ... M 12000- 5 M 12008- ... 15M 12008- 1 M 12008- ... M 12008- 5 M 12012-15M 12012- 1 M-E ...
Video: How to perform a cold start and brain dead on Smart-UPS
... perform the Cold Start and Brain Dead ... Smart- UPS The Cold start procedure is used ... determine if a UPS is functional if ... ... the Smart- Ups microprocessor. Cold Start : ... establish if a UPS will not turn ... ... use a Cold Start to troubleshoot a ... 1 ) Turn off ... the Smart- UPS from wall. ... front of the UPS until you hear ... 4) UPS should go through ... ... shows that the UPS is functioning correctly ... 5 ) You can now plug your UPS back into the ... ... is acceptable the UPS will transfer back ...
What are the computer interface port specifications for the SU and SUA Smart-UPS family?
... G Smart- UPS family? Smart- UPS ... port on the UPS . ... SUA Smart- UPS have the following ... ... Pins 3, 5 , and 6 ... ... RS-232 levels when the UPS signals that it ... The UPS will shut down ... RS-232 level is sustained on pin 1 for 4. ... The UPS responds to this ... (when the UPS is operating on ... Pin 1 is also the ... ... momentary (approximately 1 second) high RS-232 level to pin 7 ... turn on the UPS and any attached ... ... turns off the UPS and its load ... DC operating voltage is available at pin 8. Smart- UPS Communication
SRT 8 or 10kva reports Error P.11 or DC Bus Voltage Low or event codes 128/129
The UPS reports P.11 or DC Bus Voltage Low - event 128/129 ... If the problem persists, Brain dead the UPS . If the alarm reoccurs, perform a UPS Firmware upgrade to the latest 04.7 revision that addressed these issues. ... Release Notes ( UPS 04.7): ... 1 . Improved system performance of transitions between Online and Bypass operation modes. ... 3. Improved system behaviour to eliminate false detection of DC bus under voltage alarm under certain conditions. 4. Improved system handling for certain AC input conditions during system start -up.


Ergebnisse 1 - 10 von 59

Nicht gefunden, was Sie suchen?

Wenden Sie sich an unser Kundenteam, um Informationen zum technischen Support, Unterstützung bei Beschwerden und vieles mehr zu erhalten.