Video: SRT UPS reports Battery Charger Event, Event Code 142
... , or bad batteries . ... disconnect all the batteries in the system: all internal batteries and any external batteries , if used ... ... to disconnect the batteries . ... and in the Battery menu, select ... ... UPS charger or battery terminals. ... level, the batteries need to be ... SRT Li - Ion 1-1 ... ... 48V, the battery should be replaced ... SRT Li - Ion 2.2 ... ... 48V, the battery should be replaced ... ... 80v, the battery should be replaced ... ... 100v, the battery should be replaced ... ... 200v, the battery should be replaced ...