Technische FAQs

Fragen Sie uns

Die Ergebnisse filtern

    Why is my equipment dropped or rebooted while connected to my Smart-UPS?
    ... Equipment connected to Smart-UPS drops or reboots ... Smart-UPS ... attached to a Smart-UPS can be dropped ... - A UPS with a weak ... Every Smart-UPS has a " ... ... be good for 2 years if operated ... ... failure which the UPS self test may ... 2 ) ... result in unexpected UPS behavior including load drops and the UPS turning off: - Each UPS is limited in ... ... number of the UPS tells you the ... -Amp ( VA ) limit of ... ... determine if your UPS is capable of ... please use our UPS Selector Tool at
    Video: How do I configure APC Network Management Card network settings?
    Some newer Smart-UPS models provide the capability ... configure the Network Management Card 2 (NMC2) ... the front panel LCD display menu.
    How do I select the correct Smart-UPS XL battery pack for my Legacy Smart-UPS?
    " APC manufactures a wide VA range of Smart-UPS products. Some of these models
    What are the basic troubleshooting steps for the Smart-UPS smc1000-2U / smc1500-2U ?
    ... steps for the Smart-UPS smc1000- 2 U / smc1500- 2 U ? Smart-UPS smc1000- 2 U / smc1500- 2 U - All ... ... may find your UPS not functioning as ... ... Cause Solution The UPS will not turn ... ... turn on the UPS . ... note that the LCD screen may be lit even though the UPS is OFF. The UPS is not connected ... ... load to the UPS , disconnect nonessential ... ... supply to the UPS by plugging in ... ... is an internal UPS fault. ... to use the UPS .
    Smart-UPS C Series FAQ
    Smart-UPS C Series FAQ Smart-UPS ... is the new Smart-UPS C series? The Smart-UPS C series is ... new entry level Smart-UPS product designed for ... ... feature a new LCD Interface. ... models in 1000 VA and 1500 VA capacities. ... , smc1000- 2 U, smc1500- 2 U ... with the SMC Smart-UPS ? The SMC Smart-UPS only supports Powerchute ... ... not have a Smart -Slot and ... Is the LCD display the same ... SMT and SMX Smart-UPS products?
    Smart-UPS fan operation parameters
    ... run on my Smart-UPS Smart-UPS ... included on any Smart-UPS 1400 VA higher and on ... ... failure in a UPS . ... ensure that the UPS remain as cool ... ... a commercial grade UPS designed for business ... ... are operating the UPS in an overly ... ... this type of UPS . ... See your local APC reseller or APC .COM for ... ... 1. The UPS is on battery ... 2 . The UPS is charging the ... ... 3. The UPS has a load ... ... temperature of the UPS has reached greater ... ... 1. The UPS is on battery ...
    How do I update the firmware of my SMT, SMX, or SMC series Smart-UPS using the Firmware Upgrade Wizard?
    Environment: ... general, all Smart-UPS models beginning with ... ... smx1500 with firmware UPS 02.x ... ... firmware earlier than UPS 07.2 ... firmware earlier than UPS 08.0 ... the current firmware version before performing the ... ... menu of the UPS LCD screen select "About ... down to " UPS Firmware" UPS Model UPS 10.0 ... #1005) UPS 12.0 ... firmware less than UPS 08.0 ... UPS 07.1 ... Tower ( firmware UPS 08.0 ... UPS 09.4 SMT 2 U Rackmount UPS 09.4 UPS 10.1
    Why are all LED's flashing simultaneously on my Smart-UPS SU, SUA, or SURT model?
    Smart-UPS ... All non- LCD display models (Line Interactive and Online), All Serial Numbers ... All LED's, or the two center columns of LED's flashing simultaneously generally indicates a hardware failure. ... Try to reset the fault by turning the UPS off/on or by performing a "brain dead" on the unit. ... Turn off the UPS Unplug the UPS from utility power ... If this fails to clear the fault, contact APC Support for further assistance.
    How do I troubleshoot the Replace Battery LED on a Smart-UPS?
    ... lit on my Smart-UPS . Smart-UPS , Smart-UPS Online ... , or the LCD Screen on the UPS (if so ... ... for a standard UPS or 24 hours for a UPS with external batteries ... Smart-UPS products will charge ... 2 . Initiate a ... If your UPS has an LCD screen go to the ... then select " UPS Self Test" If your UPS does not have an LCD display, press ... ... warranty on all Smart-UPS products is 2 years from the ... ... visit our world wide contact page for an APC office near ...
    No power out from some outlets on a Smart-UPS
    ... outlets on a Smart-UPS Smart-UPS ... plate of the UPS . If an ... ... approximately 1/ 2 "" when ... ... tripped and your UPS features a user ... ... backplate on a Smart-UPS , please refer ... ... and SRT series Smart-UPS support switchable outlet ... the front panel LCD . From the ""Control"" menu on the UPS , you would scroll to each outlet group and choose ""TurnON - No Delay"". ... APC Application Note #177 "Software Interface for Switched Outlets and UPS Management in Smart-UPS "
    Ergebnisse 1 - 10 von 60