{}

FAQs durchsuchen

{"searchBar":{"inputPlaceholder":"Nach Stichwort suchen oder Frage stellen","searchBtn":"Suchen","error":"Bitte geben Sie ein Stichwort für die Suche ein."}}

Video: How to change the Maintenance Intervals on a Network Air FM unit

Issue:
This document contains a video on how to change the Maintenance Intervals on a Network Air FM unit.

Product line:
FM35-50, ACFM, IR40.

Environment:
All Serial Numbers.

Cause:
Install Operation.

Resolution:


How to change the Maintenance Intervals on a Network Air FM unit follow the below procedures.

1 Press ESC until you reach the main menu (On/Off).

2 Scroll to SETUP and press ENTER.

3 Scroll to SYSTEM 1 and press ENTER.

4 Press ENTER on ALARMS.

5 Press ENTER on MAINT ALARMS.

6 Press ENTER to scroll through the device available.
1 of 7 Compressors 1
2of 7 Compressor 2
3 of 7 Heaters
4 of 7 Blowers 1
5 of 7 Blowers 2
6 of 7 VFD 1
7 of 7 VFD 2

7 Press ENTER on the selected device.

8 Press the DOWN arrow once then press ENTER again.

9 Using the UP or DOWN arrows you can select the desired interval or disable this feature.

War das hilfreich?