Procházet často kladené dotazy

Are there any functional differences between the NetShelter HS and SX?

Datum publikování: 03 July 2018

Issue: 
There may be physical differences between the HS and SX models. 

Product Line: 
NetShelter SX and HS. 

Environment: 
All models, all serial numbers. 

Cause: 
Customers may want to make sure which accessories install into the new cabinet, and where. 

Resolution: 
The HS cabinet frame is higher to accommodate taller castors, but the inside dimension of the frame has not changed. 
In the NetShelter SX there are some 0U mounting spaces behind the vertical rails of the frame. These don't exist on the NetShelter HS. (see attached) 

Bylo to pro vás užitečné?

Co můžeme udělat pro zlepšení informací?

Nedaří se vám najít, co hledáte?

Náš tým zákaznické podpory vám poskytne informace o technické podpoře, pomůže řešit stížnosti a mnohem více.