Procházet často kladené dotazy



Can a full height 0U PDU be installed into the NetShelter SX Colocation cabinet?
Issue: There's a need to mount a full height 0U PDU into the NetShelter SX Colocation cabinet.
Is there a way to attach 0U PDUs to a NetShelter 2-post rack?
Issue: A customer wants to use a 0U PDU with a NetShelter 2-post rack.
Can the 0U accessory mounting brackets be installed into the front of a NetShelter SV?
Issue: Customers may want to install the 0U accessory mounting brackets into the front of a NetShelter SV cabinet.
Can vertical cable managers or 0U accessory rails be installed in the front and rear of a NetShelter SX cabinet?
Issue: Customers want to know if there is flexibility in installing vertical cable managers, or where to mount the 0U accessory rails.
How many 0U accessory channels (RCC's) are included with NetShelter SX cabinets, and how manu PDUs can fit into them?
Issue: Customers need to know how many 0U accessory channels are in each cabinet, and how many PDUs can mount into them.
Can a 0U PDU be hung upside down in the NetShelter SX cabinet?
A customer may want to install the 0U PDU with the power supply cord facing either the top or bottom of the cabinet depending ...
Can the finger-style vertical cable managers for 600 mm cabinets be installed on the same 0U Accessory Channel as a PDU?
... mm cabinets shows the cable manager being installed over both PDU mounting areas of the 0U accessory channel.
Can the center dividing section of the NetShelter SX Colocation be removed?
For various reasons, including the want to mount a particular 0U PDU, customers may wish to remove the center divider of the ...
Is there a deeper version of the AR7711?
... AR7711, but two brackets can be combined to increase the depth of the furthest 0U mounting hole to approx.
NetBotz 250 | Physical Description
2 Switched Outlet Provides power to a device at a maximum of 10 A . Activates a connected device when configured events occur.


výsledky 1 - 10 z 20

Nedaří se vám najít, co hledáte?

Náš tým zákaznické podpory vám poskytne informace o technické podpoře, pomůže řešit stížnosti a mnohem více.