Procházet často kladené dotazy



How do I upgrade and activate premium devices in StruxureOn?
... .4. X When you start using the StruxureOn ... About Premium 24 / 7 expert monitoring of your data center The Schneider Electric Service Bureau will remotely monitor all connected physical infrastructure devices 24 hours a day, 7 days a week enabling remote troubleshooting for quick resolution of critical incidents. ... Proactive service dispatch ... To upgrade a device The first time you upgrade one or more devices, you must read about pricing and accept the license agreement to continue.
PowerChute Personal Edition v3.X Error Code 2738 – Unable to install the software.
... v3. X Error Code 2738 ... ... Edition 3. X . ... Edition 3. X . ... Vista and Windows 7 operating system and ... ... · Click on Start -> All ... · Click on Start -> All Programs -> Accessories -> Command Prompt ... Considering that, plus the fact that SFC /scannow is completely automatic and very easy to use, the tool should usually be one of your first troubleshooting steps. 1. Click Start , click All Programs, click Accessories, right-click Command Prompt, and then click Run as administrator.
"Updates are available" pop up messages appear after upgrading PowerChute Personal Edition to version 3.0.2
If you are seeing updates are available pop up messages appearing after upgrading PowerChute Personal Edition 3. X to version 3.0.2 this indicates that the APC Data Service has been stopped. ... To resolve the issue restart the APC Data Service . On Windows Vista and Windows 7 go to Control Panel > Administrative Tools > Services Double click on APC Data Service and select start .
How to put PowerChute Network Shutdown version 3.1 or 4.x into debug mode?
service PowerChute start or sudo service PowerChute start
Video: How to reset the PowerChute Network Shutdown password and user name.
PowerChute Network Shutdown v3. X and 4. X ... 1. Stop the PowerChute service . ... 7 . Start the PowerChute service and log in with your new username and password.
Security Notification: "LOGJAM" vulnerability (CVE-2015-4000) - impact to PowerChute Network Shutdown.
... .2. x – These versions ... ... .0. x – DHE_ ... Java 7 may use 768 ... Java 7 may use 768 ... ... OS, Java 7 must be used ... ... .2. x – Install the ... ... .2. x will automatically detect ... V3.0. x – Install the 32-bit version of Java 8 from java.com on the machine running PowerChute. ... Once PowerChute has been configured to use Java 8 (Java 7 on Solaris x86): Stop the PowerChute service . ... Save the file and re- start the PowerChute service .
PowerChute Network Shutdown Virtual Appliance Hostname resets after reboot
PowerChute Network Shutdown Appliance 4. x &3. x ... Must stop or restart the PCNS service for the host name to change in the PCNS web interface. The commands are service PowerChute stop and service PowerChute start . ... 7 . Click OK to close the window
Migrate PowerChute Network Shutdown configuration from PowerChute v4.1, v4.2 virtual appliance to v4.3 virtual appliance
PowerChute v4.1 and v4.2 CentOS 5 virtual appliance and PowerChute v4.3 CentOS 7 virtual appliance ... If your v4.2 virtual appliance is CentOS 7 based, the steps below are not applicable. ... Log in as root and stop the PowerChute service : ... stop PowerChute. service ... On the PowerChute v4. x virtual appliance: Log in and stop the PowerChute service : ... Save the below v4. x configuration files locally from the /opt/APC/PowerChute/group1 directory: ... On the PowerChute v4.3 virtual appliance: Start the PowerChute service : start PowerChute. service
Video: How do I upgrade the firmware on an APC Network Management Card (NMC) or NMC embedded device (Rack PDU, etc)?
... v5. X . X to v6. X . X , please review ... ... v3. X . X Firmware for Smart ... ... v6. X . X Firmware for Smart ... ... firmware 3. X and Network Management ... version 5. X or 6. X firmware. ... v5. X . X to v6. X . X , please review ... 7 . Press and ... ... as 5- 7 minutes to finish ... ... will need to first upgrade to AOS ... ... then stop that service . 6. Start an XMODEM transfer ... 7 . Select option ...
Upgrading the public JRE fails When Running PowerChute Network Shutdown on Windows.
For PowerChute versions 3. X up to 4.2 Stop the PowerChute service , perform the JRE upgrade and then re- start the PowerChute service . ... Example: HKLM\SYSTEM\CurrentControlSet\ services \PCNS1 ... 7 . Another dialog will appear and PowerChute restarts.


výsledky 1 - 10 z 51

Nedaří se vám najít, co hledáte?

Náš tým zákaznické podpory vám poskytne informace o technické podpoře, pomůže řešit stížnosti a mnohem více.