Procházet často kladené dotazy



How long are the intake and exhaust hoses on the acpa4000?
The exhaust hose is 10 FT X 8 IN and yes you may have them ducted through a wall.
acpa4000 Spare Parts List
870-3640 Condenser Duct Tubing (Assy. Intake/Exhaust DUCT 10 FT X 8 IN
Where can I find Modbus Register map for Galaxy VX UPS products
Issue: Where can I find Modbus Register map for Galaxy VX UPS products
Where can I find Modbus Register map for Galaxy VX UPS products
Issue: Where can I find Modbus Register map for Galaxy VX UPS products
Default password of 1234 does not work on the Display of new Galax VX or Galaxy VM.
... of new Galax VX or Galaxy VM. Galaxy VX , Galaxy VM ... display of the Galaxy VX and VM is ... ... cable supplied with UPS Serial port setting: for 9600 bps, 8 data bits, no parity, 1 stop bit, and no flow control. ... Assuming the UPS is connected to the customer network and is granted an DHCP IP address. ... At the bottom of the screen you will a box to enter a password for “Pin [4- 8 digits]” and a “Confirm Pin 4- 8 digits]” and click on Save button.
NetBotz 750 | What parts come with the NetBotz 750?
1 NetBotz Rack Monitor 750 1 2 Wireless Coordinator ... (nbwc100u) 1 3 Brackets for ... , M4 x 8 4 5 2 ... terminal block plug 1 8 tie wraps, 203 mm ( 8 in) 2 ...
MGE STS, Galaxy 3000, 4000, 5000 and Galaxy PW; Wiring information for egx100 to any 66061-supported products
... – STS, Galaxy 3000, 4000, 5000 and Galaxy PW ... – STS, Galaxy 3000, 4000, 5000 and Galaxy PW ... for 9600, 8 , N and 1 . Slave address is 1 and wiring is ... ... This assumes only one 66061 card or UPS or STS is ... One is down ( ... ... required on the UPS /STS. The male DB9 connector is not supplied with the UPS but a black terminal block is supplied with the EGX.
Where do I find an Operation Manual for Galaxy VX Series UPS?
Issue: Operation Manual for Galaxy VX Series


výsledky 1 - 10 z 56

Nedaří se vám najít, co hledáte?

Náš tým zákaznické podpory vám poskytne informace o technické podpoře, pomůže řešit stížnosti a mnohem více.