Procházet často kladené dotazy



Can your InRow Cooling Auto-Start after a Power Failure
Can your InRow Cooling Auto- Start after a Power ... InRow The InRow RC, RD, RP and SC will start automatically if the ... The unit will go to its last known state, ie if the unit was in standby, the unit would return to standby, or if the unit is on, the unit would return to the on state. It is also possible to configure a Start up Delay of 0 to 999 seconds. ... The Display: Configure Unit >General> Startup Delay The Network Management Card Interface: Unit > Unit Configuration> Startup Delay
Can you interconnect A-Links CW and DX InRow Cooling products?
Install the terminator on the left-hand side A-link ports on the first unit .
Guidelines for installation of an acsc100, or acsc101
Receiving the unit Your InRow SC unit has been factory ... ... have received the unit in excellent condition ... crating and the unit immediately upon receipt ... ... the APC technical service department at 1 ... ... in your system start -up. The unit is manufactured with a formed steel frame for maximum strength and unit integrity. However, as with all electrical and mechanical equipment, you must take care with proper rigging of your unit . ... using a forklift, move the unit on the shipping pallet only.
Why does my InRow cooling unit keep alarming with warm start alarms
InRow , warm, starts , network, nmc, gateway, watchdog
acsc100 LCDI Cord Tripping Causes
The LCDI cord set is required when the InRow SC is used as a portable unit used on a temporary basis as described in the ...
Is the InRow ACSC1XX a precision cooling unit?
No, the SC is a cooling only unit . It does not have a humidifier or reheat.
Can I connect the ACSC1XX condenser ducts to any drop ceiling?
... sure to discuss the heat rejection needs of the InRow SC with the facilities personnel of the customer site to ensure the unit can be ...
Video: How to change the units of measure on the display of an InRow SC system
Issue: How to change the units of measure on the display of an acsc100 unit .
Video: How to change the set points in an InRow SC system
Issue: How to change the set points in an acsc100 unit .
Video: How to set the date and time on an InRow SC system
Issue: How to set the date and time on an acsc100 unit .


výsledky 1 - 10 z 69

Nedaří se vám najít, co hledáte?

Náš tým zákaznické podpory vám poskytne informace o technické podpoře, pomůže řešit stížnosti a mnohem více.