Procházet často kladené dotazy



Batteries; Is it OK to replace the internal batteries or use refurbished modular battery modules?
... PX1 20 - 80 kva , Symmetra PX2 100 kva , Symmetra PX 250 -500 kva , SUVT, ... , ais3000, Galaxy VM
Video: How to take Galaxy VM UPS out of Maintenance Bypass
Close the UIB (Unit Input Breaker) Power to the screen will come on, takes about 1 -2 minutes to boot up screen.
How to take the Single Galaxy 5000 UPS from normal operation to total power off using an external Maintenance Bypass Panel
These instructions are in the owner’s manual which can be located at Step 1 : Touch any button on the display to wake it up .
Video: How to take the Galaxy 5000 UPS from normal operation to total power off?
These instructions are in the owner’s manual which can be located at Step 1 : Touch any button on the display to wake it up .
Does the NTP need to be configured on the Galaxy VS internal NMC and the optional AP9644 NMC for all parallel or single Galaxy VS?
Issue: Does the NTP need to be configured on the Galaxy VS internal NMC and the optional AP9644 NMC for all parallel or single Galaxy VS
Modbus Installation and Troubleshooting for AP9635/AP9635CH Network Management Card 2 (NMC2)
... support Modbus TCP or Modbus RTU with AP9635/AP9635CH ( Galaxy VM, Galaxy 300 /7000, Galaxy 5000/5500, etc ...
Video: How can the Galaxy VS reduce my energy bill?
Can the Galaxy VS reduce my ... Galaxy VS ... know how the Galaxy VS can provide ... Galaxy VS is a ... Galaxy VS offers very high efficiency for small to medium data centers, buildings, and facilities. ... Galaxy VS offers 99% efficiency in patented ECOnversion mode. ... World-class efficiency up to 99% ... Compliant with IEC 62040-3 Class 1 output performance of UPS standard ... Explore the Galaxy VS in 3D!


výsledky 1 - 10 z 54

Nedaří se vám najít, co hledáte?

Náš tým zákaznické podpory vám poskytne informace o technické podpoře, pomůže řešit stížnosti a mnohem více.