Procházet často kladené dotazy



SMTP Port option in PowerChute Business Edition version 9.2, 9.5, 10.x
... 5, & 10 .x Agent The following five fields must be ... ... methods mentioned: its name, its ipv4 address, or its ipv6 address. It is the e-mail account to be used to send notifications. ... Port numbers can have a maximum of five digits and can be set to 25, 465, 587, or any number ranging from 5000 to 32768. ... The Console is not available with PCBE Agent 9.5 or 10 .x ... You can enable it by selecting the Basic E-Mail for Authentication
Why is my equipment dropped or rebooted while connected to my Smart-UPS?
... good for 2 years if operated at ... ... be plugged into it . ... printer connected to it . The computer ... 5 ) It will begin with ... followed by 4 digits and sometimes a ... ... UPS thus causing it to shutdown and ... ... to battery, it may have an ... Please keep in mind that this is very uncommon with IT equipment. ... With either type of connection it is important to ensure that wires are firmly connected and that EPO connections are not being run in parallel or daisy chained. Each UPS must have its ' own pair of wires running back to the EPO switch.
Runtime Calibration feature requirements for SMX/SMT units
... working properly, it is either refused ... ... required load is 10 % (SMX ... %; with 5 or more XBPs ... It is recommended not to perform more than one or two runtime calibrations per year , as frequent battery calibrations can significantly decrease the life expectancy of the battery. ... It is important to note that the actual run time during a power outage is not affected by whether a run time calibration had been performed, as the actual run time is dependent on the physical power
Frequently Asked Questions for the new Lithium-ion Smart-UPS products.
Is it safe to use ... Cycle life refers to the number of times a battery can expect to be fully discharged and recharged within a specified temperature range before it needs to be replaced. ... The UPS warranty is 5 years for both the electronics and the internal batteries. ... So it is possible to replace the internal batteries while the UPS is operating in online mode. How likely is it that I will need to replace my batteries under normal circumstances? ... The lifecycle of the UPS is approximately 10 years . ... It is recommended that the UPS be replaced with a new model.
NetBotz History Export date is seen as a Linux Time Stamp
... such much of it's data uses a ... It is unlikely this will be changed in a future revision so if it is necessary to view this as a date, the information can always be imported into a spread sheet application such as Microsoft Excel. ... I must delete the last 3 digits just to be able to use the suggested Excel formulae: ... =(((LEFT(C2, 10 )/60)/60)/24)+DATE(1970,1,1) ... 6/ 5 /16 3:27 AM
What are the factors that affect Battery Rated Service Life?
On paper, batteries are given a design life of 5 years , 8 years , 10 years , etc. They get weak, ...
Why are the Trigger Alarm and Run Self Test buttons grayed out for my unit on the SmartConnect web portal?
Once the change has been made it will take a 5 to 10 minutes for the change to take affect and the web browser will ...
Why isn’t snmpv3 working properly in Network Management Card AOS versions 3.5.7 and earlier?
Upon rebooting, the NMC will take about 5 - 10 minutes to complete its backend processes needed in order to enable snmpv3.
Data Center Expert | Troubleshooting SNMP Lost Communication to Third Party Devices
If having regular intermittent lost communications, it is recommended to increase the values to 10 second Timeouts and 5 Retries.
Data Center Expert | Troubleshooting SNMP Lost Communication to APC Devices
NOTE: If having regular intermittent lost communications, it is recommended to increase the values to 10 second Timeouts and 5 Retries.


výsledky 1 - 10 z 83

Nedaří se vám najít, co hledáte?

Náš tým zákaznické podpory vám poskytne informace o technické podpoře, pomůže řešit stížnosti a mnohem více.