Procházet často kladené dotazy



NetBotz v3 | Security Information
Should only be open temporarily for support reasons. SMTP TCP 25 Outbound - Not configured by default Network requirements are low.
Does the Shellshock Vulnerability affect APC products?
NetBotz Appliances ... - On 25 -SEP-2014, the GNU Bourne Again Shell (Bash) Vulnerability, also called the "Shellshock" Vulnerability (CVE-2014-6271 and CVE-2014-7169) was detected and published by several Cyber Security outlets ... NetBotz Appliances do not utilize BASH and is therefore not affected.
USB Specifications for the WallBotz 500
NetBotz ... NetBotz 500 nbwl0500 ... WallBotz 500 USB Specifications 4 chained hubs up to 80 feet ( 25 meters) ... 4 chained together with standard USB cable on the end going to the USB device (80 feet / 25 meters)
How To: Configuring an APC Network Management Card with popular email services such as Gmail, Yahoo!, Office 365, and Hotmail/Outlook.com
... , ap9340, NetBotz 200) If the instructions above do not work, please ensure that TCP port 25 is open. ... As a result, many ISP's block port 25 since it has been used for the transmission of spam and malware from infected computers for nearly a decade. Another ... If this does not work, please ensure that port 25 is open (or whatever port your email provider uses), verify you've obtained the correct settings from your email provider, your outgoing From Address
Network Management Card (NMC) Password Reset Procedure
Devices with an embedded Network Management Card 1 include (but are not limited to): Metered/Switched Rack PDUs (AP78XX, AP79XX), Rack Automatic Transfer Switches (AP77XX, Environmental Monitoring Units (ap9320, ap9340, NetBotz 200) ... NetBotz 200/Environmental Monitoring (AP9319, ap9340, ap9320) ... NetBotz 200/Environmental Monitoring (AP9319, ap9340, ap9320) ... Hold down the Reset button for 20- 25 seconds, ensuring the Status LED is pulsing green during this time.
How do I troubleshoot email failures on a Network Management Card?
Devices with an embedded Network Management Card 1 include (but are not limited to): Metered/Switched Rack PDUs (AP78XX, AP79XX), Rack Automatic Transfer Switches (AP77XX, Environmental Monitoring Units (ap9320, ap9340, NetBotz 200) ... You can test this by connecting to the email server using Telnet over SMTP port 25 and see if it gives a username/password prompt.
What HID cards supported by NetBotz rack access AP9361, nbpd0170 pod, and NetBotz 250.
The Rack Monitor 250 with the NetBotz 125 kHz Handle Kit (nbhn0125) supports the following 125khz proximity cards:
NetBotz | End of Sale & End of Support Information
... January 2017 January 2019 nbrk0250 nbrk0200 / nbrk0201 NetBotz Rack Monitor 200 October 2016 October 2018 nbrk0250 ap9360 Proximity Card Rack Lock Kit August 2007 ...


výsledky 1 - 10 z 54

Nedaří se vám najít, co hledáte?

Náš tým zákaznické podpory vám poskytne informace o technické podpoře, pomůže řešit stížnosti a mnohem více.