Procházet často kladené dotazy



Why might the Overload LED be lit on my APC Back-UPS?
All APC Back-UPS Product Families. ... All APC Back-UPS Product Families. ... Each model of Back-UPS is capable of handling up to a certain amount of equipment. ... is rated for 500 Volt Amps (or 315 Watts). Verify that your equipment plugged into the Battery Backup outlets does not exceed the VA rating (denoted by the number in the APC's UPS Sizing Tool ... Try moving one or more pieces of equipment to the Surge Protection outlets . ... contact APC's Technical Support ... contact APC's Technical Support
APC Recall for the Back-UPS CS (120v and 230v); How do I know if my unit is one of the affected units?
The affected CS 350 and CS 500 models were manufactured between November 2000 ... primarily through distributors, catalog and retail outlets in North America.
What is AVR (Automatic Voltage Regulation)?
APC Back-UPS , APC Smart-UPS
Why might the LEDs on my Back-UPS or Smart-UPS SC be flashing?
... LED lights on Back-UPS Pro, Back-UPS Pro USB, Back-UPS LS, and ... Back-UPS Pro, Back-UPS USB, Back-UPS LS, Back-UPS CS, Back-UPS NS/XS ... ... included with your Back-UPS Pro after it ... ... power from your wall socket . APC UPS Selector tool ... the Battery Backup outlets is drawing more ... ... Each model of Back-UPS Pro is capable ... ... is rated for 500 Volt Amps ( ... ... battery backed up outlets "" does ... ... Only"" outlets .
Recommendations for protecting a laser printer
in to its Surge Only Outlets . These low voltage situations may cause an APC Back-UPS to transfer to battery operation repeatedly, ...
Which steps should I take for installing and configuring my NEW APC Back-UPS?
If it turns out you have more things that need a surge only outlet it is recommended that you purchase an APC surge arrest.
What are the features of the switched outlet groups on my SMT, SMX, or SRT Smart-UPS?
Some APC Back-UPS models allow for a master ... on a device in one outlet will cause a second outlet to power on.
Video: Why might my APC Back-UPS Product be beeping?
... UPS is not being overloaded (refer to the Back-UPS products User Manual for watt capacity of the battery outlets ).
Why is my APC Back-UPS giving a single beep every 5 seconds?
When the voltage returns to normal the Back-UPS will wake up and restore power to the battery outlets .
Why is my Back-UPS ES giving a Constant tone with the Power on LED flashing?
APC recommends plugging only the ... in the battery powered outlets , other peripherals ... Only"" outlets on the labeled on the the UPS.


výsledky 1 - 10 z 59

Nedaří se vám najít, co hledáte?

Náš tým zákaznické podpory vám poskytne informace o technické podpoře, pomůže řešit stížnosti a mnohem více.