{}

Prohledejte časté dotazy

{"searchBar":{"inputPlaceholder":"Hledejte podle klíčového slova nebo se zeptejte","searchBtn":"Hledat","error":"Zadejte klíčové slovo pro hledání"}}

How to configure NetBotz version 2 external sensors?

Issue:
Netbotz External Sensor Installation Tips

Product Line:
Netbotz

Environment:
NetBotz 2.x

Cause:
Configuration tips.

Resolution:

Adding sensors that connect to the external sensor ports require configuration before they will function. Follow these basic guidelines when adding sensors to the external sensor ports:
  • Physically connect the add-on sensor using and noting the external sensor port(s)
  • Under “Configuration” in the Advanced View, click on “Sensor Pods”. Select the appropriate Sensor Pod where you attached the sensor
  • Click “External Ports” and select the appropriate sensor and the port that it’s plugged into, then name it appropriately
  • Once that’s done, you can then select the “Sensors” button and edit the thresholds for that device accordingly
  • It’s always a good idea to test the sensors and cabling before fully deploying the solution on-site.

Bylo to užitečné?

Zjistěte více
Zjistěte více