Browse FAQs



Video: How do I upgrade the firmware on an APC Network Management Card (NMC) or NMC embedded device (Rack PDU, etc)?
... unit with an embedded NMC that you ... ... Devices with an embedded Web/SNMP ... ... Devices with an embedded Network Management Card ... ... Devices with an embedded Network Management Card ... ... devices that have embedded (mini) ... ... , and Default Gateway and attached to ... ... window on a PC which is connected ... 1. To perform a firmware flash with this method the Management Card must have been previously configured with a System IP, Subnet Mask, and Default Gateway and attached to the network. ... 2. Open an MS-DOS command prompt window on a PC which is connected to the network.
Uniflair BACnet (Building Automation and Control Networks)
• 120ω resistor; PC for the gateway configuration
Modbus communication on a Uniflair unit.
• 1 terminal line (120 ω); PC for the gateway configuration.
Why Node-red embedded with Ecostruxure Augmented Operator Advisor stop few second after starting?
Go to …Schneider-electric \ Ecostruxure Augmented Operator Advisor \ Node-red \ node-red home
New demo available: IT Expert and EcoStruxure IT app
IT Expert demo ... based on a real organization with real data, demonstrating IT Expert functionality in a preconfigured environment - no signup required!
Why is my Network Management Card's default gateway showing as 0.0.0.0 under Current ipv4 settings?
Devices with an embedded Network Management Card 1 include (but are not limited to): Metered/Switched Rack PDUs (AP78XX, ...
How can I mass configure a Network Management Card (NMC) or NMC embedded product?
How can I mass configure a Network Management Card (NMC) or NMC embedded product? IP address, Subnet Mask, Default Gateway , and Boot Mode cannot be modified through the config.ini
How do I recover the firmware on an ap5610, AP5615, AP5616 Digital IP KVM models?
Reconfigure the PC to have a static/manual IP address of ... .0.0.0, no default gateway is required.
How do I retrieve logs from my Secure-UPS XP1K9NN42RCC Power management Unit?
How to create a direct connection between a computer and a PMU’s (Power management unit) embedded network management card (NMC) ... Set the default gateway of the NMC as the IP address of the computer. ... The embedded NMC will restart after the configuration change. ... Default gateway : 192.168.1.2 (which is the IP address of the NMC)
How to assign a fixed IP address to SmartConnect enabled Smart-UPS
SMTL, SMT and SMC, model Smart-UPS with embedded SmartConnect network port. ... Smart-UPS with embedded SmartConnect network port ... From the UPS IP Address Setting menu you can change from DHCP to Manual and enter a static IP address, subnet mask, gateway , and DNS. ... To set a fix IP address for the embedded SmartConnect network port you must log into the router the UPS is connected to via the network.


Results 1 - 10 of 50

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.