Technical FAQs

Ask a Question

Filter results

    Can a full height 0U PDU be installed into the NetShelter SX Colocation cabinet?
    Issue: Some customers may want to mount a full height 0U PDU into the NetShelter SX Colocation cabinet.
    Can a 0U PDU be hung upside down in the NetShelter SX cabinet?
    Customers may want to install the 0U PDU with the power supply cord facing either the top or bottom of the cabinet depending upon ...
    Can the center dividing section of the NetShelter SX Colocation be removed?
    For various reasons, including the want to mount a particular 0U PDU , customers may wish to remove the center divider of the ...
    Is there a way to attach 0U PDUs to a NetShelter 2-post rack?
    A customer wants to use a 0U PDU with a NetShelter 2-post rack. ... The 2-post rack doesn't have an accessory to attach to the side and hand 0U PDUs. ... The User Manual shows several ways to attach the bracket to racks and cabinets.
    Differences between ap7xxx and ap7xxxb Series Rack PDU's
    Discontinued: Metered AP7851 - RackPDU,Metered, 0U AP7851
    Can the finger-style vertical cable managers for 600 mm cabinets be installed on the same 0U Accessory Channel as a PDU?
    ... for 600 mm cabinets shows the cable manager being installed over both PDU mounting areas of the 0U accessory channel.
    Is there a deeper version of the AR7711?
    ... a deeper version of the AR7711, but two brackets can be combined to increase the depth of the furthest 0U mounting hole to ...
    Can the 0U accessory mounting brackets be installed into the front of a NetShelter SV?
    ... , ar2500, ar2507, ar2580, ar2587, ar2200, ar2280, accessory, bracket , front,
    Results 1 - 10 of 50