Browse FAQs

InRoom Clearing the communication bus

Published date: 22 July 2020

Oftentimes if an InRoom unit, or group of units, is experiencing communication faults or other erroneous alarms, clearing the I/O bus will quickly and easily resolve the issue.

This can be done by pressing the right arrow repeatedly until the entire screen is selected (all blacked out), and then pressing the OK button.  You will be prompted for the password at this point (the default password is either 0000 or 2718).  Enter the password to complete the process.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.