What is the NetBotz smoke sensor NBES0307 sensitivity?
Published date:
16 July 2020
Issue:
What is the NetBotz smoke sensor sensitivity?
Product Line:
NetBotz sensors
Environment:
NetBotz smoke sensor NBES0307
Cause:
Customer request for sensor sensitivity.
Resolution:
The nominal detection sensitivity for the NBES0307 is 2.5 percent-obscuration-per-foot. This is not configurable on the sensor and the NetBotz appliance will only see the sensor as a state sensor...smoke or no smoke. A variable threshold (such as those available for a numeric sensor such as temperature) is not possible.
Please see the attached datasheet for more smoke sensor information. Please see the NetBotz product page for more recent documentation.