Cause:
Potential configuration issues on the Servertech PDU may prevent device discovery using SNMPv3 if authentication is set.
Resolution:
During discovery in Data Center Expert, it was seen that changing the "trap type" on the PDU to snmpv3 allowed DCE to discover the device. NOTE: During discovery of 3rd party devices, the priority scanning" option should be unchecked.
Can't find what you are looking for?
Reach out to our customer care team to receive information on technical support, assistance for complaints and more.