Browse FAQs

What are the pinouts of the RJ45 sensor connectors on a NetBotz appliance?

Published date: 21 July 2020

Issue:
RJ45 Connector Pin Outs For the Netbotz Appliances

Product Line:
NetBotz

Environment: 
NetBotz version 3 sensor cables

Cause:
Pin-out specifications.

Resolution:

-NetBotz does not release the pin outs for the RJ45 connectors for any sensors designed for NetBotz Appliances.

-To address this issue, NetBotz sells a standard dry contact cable that is our RJ45 connector one end and two bare dry contact style wires on the other.

-This cable is provided to allow customers to attach our NetBotz Appliances to any dry contact type connection without having to have the RJ45 connector pin outs.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.