Browse FAQs

What Services and or Warranty are available for an EcoAisle

Published date: 18 July 2020


Issue:  
What Services and or Warranty are available for an EcoAisle 

Product line:
EcoAisle.

Environment: 
Only ACRC100, EcoBreeze, ACRC301X.

Cause:   
Install. 

Resolution:  Warranty: One year parts only. 

 

•         Dual Row Ceiling Panel Containment install service

•         SE will assemble and mount the ceiling panel containment system onto the racks

•         Air Return / Ducted install service

•         SE will assemble and mount the adjustable mounts and the base frame onto the racks

•         The duct panels and cross aisle beams at the top of the duct will have to utilize contractors to complete the installation. 

•         SE will install the duct panels up to a 9 ft ceiling. 

•         Over 9ft will require contractor support.

•         Single Row Ceiling Panel Containment install service

•         SE will assemble and mount the ceiling panel containment with the exception of the wall mounting rail

•         Wall mounting rail will require contractor support to attach the rail to the w Dual Row Ceiling Panel Containment install service

•         SE will assemble and mount the ceiling panel containment system onto the racks

•         Air Return / Ducted install service

•         SE will assemble and mount the adjustable mounts and the base frame onto the racks

•         The duct panels and cross aisle beams at the top of the duct will have to utilize contractors to complete the installation. 

•         SE will install the duct panels up to a 9 ft ceiling. 

•         Over 9ft will require contractor support.

•         Single Row Ceiling Panel Containment install service

•         SE will assemble and mount the ceiling panel containment with the exception of the wall mounting rail

•         Wall mounting rail will require contractor support to attach the rail to the wall structure of the room

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.