Browse FAQs

BMS AP9921X-AP9922; alarms “Battery High Chemistry Voltage”

Published date: 22 July 2020

 
 
 
Issue:
BMS AP9921X-AP9922; alarms “Battery High Chemistry Voltage”

 
Product line:
Battery Management System (BMS) AP9921X & AP9922

 
Environment:
All models, all serial numbers

 
Cause:
The voltage of a battery is above the threshold for the battery type.

 
Resolution:
If a specific battery causes repeated alarms (especially if the voltage continues to increase), the battery is failing. Replace the battery.
 
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.