Browse FAQs

Pelco camera presets configured on the NetBotz appliance are saved on the camera using a default naming convention

Published date: 22 July 2020

Issue:

Pelco camera presets configured on the NetBotz appliance are saved on the camera using a default naming convention rather than the preset names configured in the NetBotz appliance user interface.

Product Line:

NetBotz, Pelco

Environment:

NetBotz, Pelco

Cause:

This is a known limitation of the integration between the NetBotz appliance and Pelco cameras.

Resolution:

There is no resolution at this time.
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.