Browse FAQs

How to troubleshoot a Rack Inlet High Temp Alarm

Published date: 18 July 2020

Issue:

Rack inlet high alarm

 

Product line:

Inrow

 

Environment:

Data Center Inrow

 

Cause:

Temp threshold is to low or sensor is in wrong place

 

Resolution:

Check threshold and check placement of sensor. Threshold should be at least 3 degrees above max normal temp and sensor should be place in the front of the server rack at least 6 inches from front of the server with blanking panels in any gaps in the rack

 


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.