Browse FAQs

Data Center Expert | Surveillance frame rate when NetBotz communication is SSL

Published date: 23 July 2020

Issue:
StruxureWare Data Center Expert surveillance slows when communicating to NetBotz appliance(s) using SSL.

Product Line:
InfraStruXure Central (ISXC)
StruxureWare Data Center Expert (DCE)
NetBotz (series 300 and higher)

Environment:
InfraStruXure Central (all verisons)
StruxureWare Data Center Expert (all verisons)
NetBotz (all versions)

Cause:
Regardless of the frame rate you have set within the Data Center Expert surveillance settings, the maximum frame rate Data Center Expert will receive from a NetBotz appliance is 5 frames per second. This is due to the overhead that SSL creates.

Resolution:
This is working as designed. Without the encryption and decryption in SSL, surveillance frame rates will remain as configured. This issue effects both version 2 and version 3 NetBotz appliances.
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.