Consultar las preguntas frecuentes

​Video: How to Remove the Battery Blanking Panel on a Galaxy 3500 and Smart-UPS VT UPS

Fecha de publicación: 10 May 2018

Issue:
Removing Top Battery Blanking Panel on Smart-UPS VT and Galaxy 3500

Product line:
Galaxy 3500 and Smart-UPS VT UPS

Environment:
All Product models, all serial numbers
 
Cause:
The blanking panel must be remove to install batteries or to close up a battery row that no longer hosts batteries.

Resolution:
All Battery panels are held in by two screws at the bottom edge of the panel, but the top panel has an additional step as it interacts with the power module slide tray located above it.
 
Once the two screws are removed you will need to pull the panel forward along the lower lip of the power module slide tray until it reaches the slot to allow it to fall out.

The following video demonstrates this procedure:
 

¿Ha sido útil?

¿Qué podemos hacer para mejorar la información?

¿No encuentras lo que buscas?

Ponte en contacto con nuestro equipo de atención al cliente para obtener información sobre asistencia técnica, asistencia para quejas, etc.