Consultar las preguntas frecuentes

How to clear the password on the Matrix-UPS display?

Fecha de publicación: 27 May 2014



Issue

How to reset the password of a Matrix UPS LCD display

Product Line

Matrix UPS

Environment

All serial ranges


Cause

The user has the option of password protecting the display to prevent tampering.  In rare instances a communication error may occur within the Electronics Unit of the Matrix resulting in this as well.


Resolution

Reset the Electronics Unit (EU, the top half of the Matrix) by placing the Matrix into bypass using the rear panel rocker switch (see User's Manual) and unscrewing the rear bypass screw. (This is the big screw located on the rear of the unit between the top half, EU, and lower half, IU.) Now, reconnect the bypass screw and bring the Matrix out of bypass by moving the rocker switch back to its original position. Upon resetting the Matrix, you should have full access to the menus. If the problem persists or is seen on a recurring basis, the logic in the Electronics Unit may be faulty.






¿Ha sido útil?

¿Qué podemos hacer para mejorar la información?

¿No encuentras lo que buscas?

Ponte en contacto con nuestro equipo de atención al cliente para obtener información sobre asistencia técnica, asistencia para quejas, etc.