Consultar las preguntas frecuentes



Hardwiring to 120v, 208v, and 240v loads from a 208v/240v SmartUPS RT UPS
... 240v loads from a 208v/240v ... ... do not require a stepdown transformer to ... ... outputs and require a transformer to supply ... ... UPS RT is a single phase UPS with a 3 wire unbalanced ... ... 2 hots and a ground on the ... 2 hots and a ground on the ... ... do not use a neutral. They require a stepdown transformer to ... loads and provide a Neutral ... you will see 208 volts (or 240v ... not two balanced 120 volt legs as you ... ... hardwire out to a 120v load without the use of a transformer will result ...
Single Phase Symmetra Drops the Load When Returning from Bypass
Input Voltage: Line I 132.7, Line II 132.7, LI-LII 230 VAC Output Voltage Setting: 208 V
Video: How do I configure a 208v Smart-UPS RT or SRT for use with a 240v input?
If you need 120 v for your equipment you will still need to use a stepdown transformer.
How do I update the firmware of my SRT, SMC, XU, XP, SMX, SMT, SMTL, SCL, SRC, CHS series Smart-UPS?
Devices that do *NOT* have upgradable firmware: These units are 120 V devices built prior to date code 1037. Date code is the first 4 numbers in your serial number.
How do I update the firmware of my SRT/SMC/XU/XP/SMX/SMT/SCL/SRC/CHS series Smart-UPS using the Firmware Upgrade Wizard?
Issue: These units are 120 V devices built prior to date code 1037. Date code is the first 4 numbers in your serial number.
What are the basic troubleshooting steps for the Smart-UPS smx1500rm2u ?
If the UPS indicates a site wiring fault, have a qualified electrician inspect the building wiring. (Applicable for 120 V units only.)
What are the basic troubleshooting steps for the Smart-UPS smx2000hv / smx3000hv ?
If the UPS indicates a site wiring fault, have a qualified electrician inspect the building wiring. (Applicable for 120 V units only.)
What are the basic troubleshooting steps for the Smart-UPS smx2000lv / smx3000lv ?
If the UPS indicates a site wiring fault, have a qualified electrician inspect the building wiring. (Applicable for 120 V units only.)
What are the basic troubleshooting steps for the Smart-UPS smc1000 / smc1500 ?
If the UPS indicates a site wiring fault, have a qualified electrician inspect the building wiring. (Applicable for 120 V units only.)
What are the basic troubleshooting steps for the Smart-UPS smx2000rmhv2u / smx3000rmhv2u ?
If the UPS indicates a site wiring fault, have a qualified electrician inspect the building wiring. (Applicable for 120 V units only.)


Resultados 1 - 10 de 50

¿No encuentras lo que buscas?

Ponte en contacto con nuestro equipo de atención al cliente para obtener información sobre asistencia técnica, asistencia para quejas, etc.