Consultar las preguntas frecuentes



Hardwiring to 120v, 208v, and 240v loads from a 208v/240v SmartUPS RT UPS
... 240v loads from a 208v/240v ... These two models are split ... do not require a stepdown transformer to ... ... outputs and require a transformer to supply ... ... UPS RT is a single phase UPS with a 3 wire unbalanced ... They require 2 hots and a ground on the input, and 2 hots and a ground on the ... ... do not use a neutral. They require a stepdown transformer to ... loads and provide a Neutral ... you will see 208 volts (or 240v ... it is not two balanced 120 volt legs as you ... The two output legs are ...
Single Phase Symmetra Drops the Load When Returning from Bypass
Input Voltage: Line I 132.7, Line II 132.7, LI-LII 230 VAC Output Voltage Setting: 208 V
What are the basic troubleshooting steps for the Smart-UPS smc1000-2U / smc1500-2U ?
If the UPS indicates a site wiring fault, have a qualified electrician inspect the building wiring. (Applicable for 120 V units only.)
Video: How do I configure a 208v Smart-UPS RT or SRT for use with a 240v input?
If you need 120 v for your equipment you will still need to use a stepdown transformer.
How do I update the firmware of my SRT, SMC, XU, XP, SMX, SMT, SMTL, SCL, SRC, CHS series Smart-UPS?
Devices that do *NOT* have upgradable firmware: These units are 120 V devices built prior to date code 1037. Date code is the first 4 numbers in your serial number.
How do I update the firmware of my SRT/SMC/XU/XP/SMX/SMT/SCL/SRC/CHS series Smart-UPS using the Firmware Upgrade Wizard?
Issue: These units are 120 V devices built prior to date code 1037. Date code is the first 4 numbers in your serial number.
What are the basic troubleshooting steps for the Smart-UPS smx1500rm2u ?
If the UPS indicates a site wiring fault, have a qualified electrician inspect the building wiring. (Applicable for 120 V units only.)
What are the basic troubleshooting steps for the Smart-UPS smx2000hv / smx3000hv ?
If the UPS indicates a site wiring fault, have a qualified electrician inspect the building wiring. (Applicable for 120 V units only.)
What are the basic troubleshooting steps for the Smart-UPS smx2000lv / smx3000lv ?
If the UPS indicates a site wiring fault, have a qualified electrician inspect the building wiring. (Applicable for 120 V units only.)
What are the basic troubleshooting steps for the Smart-UPS smc1000 / smc1500 ?
If the UPS indicates a site wiring fault, have a qualified electrician inspect the building wiring. (Applicable for 120 V units only.)


Resultados 1 - 10 de 63

¿No encuentras lo que buscas?

Ponte en contacto con nuestro equipo de atención al cliente para obtener información sobre asistencia técnica, asistencia para quejas, etc.