Consultar las preguntas frecuentes



Spare parts list for ACRD1XX, and ACRD2XX
1 /2"ODM X 5 / 8 " ODF EXTENDED, r410a 3 TON - SPARE PART 0.656 160.0 ...
Network Air FM unit spare parts list
875-1059/875-1057a TXV 5 / 8 " X 1 - 1 / 8 " R22 - (FM NEW ACFM MODELS )
NetBotz 750 | What parts come with the NetBotz 750?
1 NetBotz Rack Monitor 750 1 2 Wireless Coordinator ... (nbwc100u) 1 3 Brackets for ... , M4 x 8 4 5 2-position ... terminal block plug 1 8 tie wraps, 203 mm ( 8 in) 2 ...
Symmetra LX Seismic Anchoring for Tower Models
( 8 ) 812-0011a - 5 /16" 18 thread count x 1 " long Bolts used to attach L-bracket ...
Are NetShelter SX, SV, CX or VX cabinets NEMA rated?
nema 1 , nema 2 ... , nema 3 x , nema 3 ... , nema 4 x , nema 5 , nema 6 ... 7, nema 8 , nema 9 ...
ACSC1XX Spare Parts List
1 ... BRACKET SCREW M 5 X 12 FLT UCUT PHIL M 5 X 12 BLK ( ... 1 1 1 1 ... MTL PPR 400v 5 % 40uf RD ... ... -230/ 1 /60 ( ... ... -240/ 1 /50 ( ... ... -230/ 1 /60, ... 1 ... -240/ 1 /50 SC ... 1 ... .13" X .13" X .13" ... .19" X .19" X .19" 1 1 1 1 ... , 3/ 8 " ODF ( ... 1 1 ... WASHABLE IR SERIES 1 /2" ...
How to configure the SRC 5,6,8 & 10 KVA UPS Models External Battery Packs using the LCD display
All SRC models , All Serial ... 1 . Press the ... 5 . Enter the ... ... of battery) x (total number ... Example 1 : If there ... ... series(for 5 KVA), ... is 100 AH x 16 pcs= ... The 80ah inside the table is the default setting for 5kva/6kva ( 1 EXB: 16pcs of 5ah battery) The default setting for 8kva is 140ah ( 1 EXB: 20pcs of 7ah battery) The default setting for 10kva is 180ah ( 1 EXB: 20pcs of 9ah battery).
How to enable .NET 2.0 on Windows 8.x and 10
Windows 8 . x and 10 ... 1 . Open up the control panel. (Right click start - then click control panel) ... 5 . You should see .NET Framework 3.5 (includes .NET
How to take the Single Galaxy 5000 UPS from normal operation to total power off using an external Maintenance Bypass Panel
... to take the Single Galaxy 5000 UPS ... All models , all serial numbers ... This procedure is for a single UPS with an external maintenance bypass panel. Regardless of wall mount, or free standing, the external breakers have the same designation. ... Step 1 : Touch any button on the display to wake it up. ... Step 5 : Press the Inverter OFF (gray) button for 3 seconds to transfer the load to the Static Bypass Switch. ... Step 8 : Unlock CB2, remove the key, and place it in the key interlock. ... Turn off Q 1 Switch
APC Schneider Cooling Unit Identification
All Product models , all serial ... Model X = No Reheat ... X =No Humidifier ... Model X = No Reheat ... X = No Humidifier ... Model X = No Reheat ... X = No Humidifier ... In-Row Model X = No Reheat ... X = No Humidifier ... Model ... AFX 018 ( 5 T) X = No Reheat ... X = No Humidifier ... ... -XXX- X Model 27 ( 8 T) ... -XXX- X -XX Model AFX 1 = 1 Bay ... Bay 06 ( 1 Bay) 08 ( 1 Bay)


Resultados 1 - 10 de 97

¿No encuentras lo que buscas?

Ponte en contacto con nuestro equipo de atención al cliente para obtener información sobre asistencia técnica, asistencia para quejas, etc.