Consultar las preguntas frecuentes



MGE STS, Galaxy 3000, 4000, 5000 and Galaxy PW; Wiring information for egx100 to any 66061-supported products
The 66061 JBUS/Modbus card is configured for 9600, 8 , N and 1 . Slave address is 1 and wiring is 2 ...
Default password of 1234 does not work on the Display of new Galax VX or Galaxy VM.
Serial port setting: for 9600 bps, 8 data bits, no parity, 1 stop bit, and no flow control.
Which SmartSlot accessories are supported by the Galaxy 3500 (g3500) UPS?
2.) Utilize an APC ap9600 single slot SmartSlot expansion chassis and extend the cable to the ap9600 with a 940- 1500 serial ...
Galaxy VX; How to configure the Network Communications options
Resolution: The network can be configured for the display and for the cards in Smart Slot 1 and
How do I connect a EPO (Emergency Power Off) circuit to Galaxy VX?
... apcmedia.com/salestools/MBPN-A35JB8/MBPN-A35JB8_R 1 _EN.pdf?sdirect=true
Galaxy VX; What is the Airflow and BTU heat dissipation?
... /hr and CFM for the same four load level (three at 30c and one at 40c) as the heat dissipation (BTU ...
Information regarding the Aluminum cable for the Galaxy VX products
Cause: Recommended Aluminum Cables for 1250kw – 1500 KW
Where can I find Modbus Register map for Galaxy VX UPS products
Issue: Where can I find Modbus Register map for Galaxy VX UPS products


Resultados 1 - 10 de 50

¿No encuentras lo que buscas?

Ponte en contacto con nuestro equipo de atención al cliente para obtener información sobre asistencia técnica, asistencia para quejas, etc.