Consultar las preguntas frecuentes



Data Center Expert | What virtualization environments are supported?
... the Data Center Expert virtual appliance? ... StruxureWare Data Center Expert (DCE) ... StruxureWare Data Center Expert (all verisons ... ... found within the EcoStruxure IT Help Center at ... ... -Center- Expert -Virtual- ... ... The Data Center Expert v7. ... ... to five device nodes and one surveillance node . ... monitor additional device nodes and activate supported ... ... the Data Center Expert 7.2 ... The Data Center Expert virtual appliance is delivered as an OVA (Open Virtualization Archive), expected to function properly on any virtualization platform that supports this format, or has an appropriate converter utility.
Data Center Expert | How do hardware and software support contracts work?
... StruxureWare Data Center Expert . ... StruxureWare Data Center Expert (DCE) ... StruxureWare Data Center Expert (all versions ... ... StruxureWare Data Center Expert appliances come with 2 years of factory hardware ... ... The Data Center Expert appliance and any ... ... a default 25 nodes (covered under ... as each additional node license. ... StruxureWare Data Center Expert Appliances can have ... total of 5 years , which includes 2 years of factory warranty ... Year 1 Year 2 Year 3 Year 4 Year 5 Year 6 ... virtual appliance until it is activated using ... ... ASMNS5_R 1 _EN. ...
Data Center Expert | Why does StruxureWare not accept my One Time passcode?
... StruxureWare Data Center Expert is not accepting ... ... StruxureWare Data Center Expert (DCE) ... ... StruxureWare Data Center Expert (all versions ... ... SturuxureWare Data Center Expert requires a 64 ... the Data Center Expert's MAC address. ... StruxureWare Data Center Expert (DCE) ... 1 . In a ... ... StruxureWare Data Center Expert Basic ... StruxureWare Data Center Expert Standard ... StruxureWare Data Center Expert Enterprise ... StruxureWare Data Center Expert Virtual Machine ... wish to associate it with and click ... ... verify that the node count is correct ... 10 . ... asset by pasting it into a word ... 11. Launch your Expert client. ... 14. Paste the license key(s) one at a time into the popup box.
Data Center Expert | Migrating from a Physical Appliance to a Virtual Appliance
... Note that if your previous server already has licensing on it (beyond the base 25 device nodes and 1 surveillance node ) your will ...
Data Center Expert | Trial version VM appears to have 25 nodes available.
This is by design. It was done so APC did not need to add a 5 node key to just this one version.
Can StruxureWare Data Center Expert output a 32 bit register with its Modbus output?
A single register in StruxureWare Data Center Expert's modbus output is ... ... StruxureWare Data center Expert ... StruxureWare Data center Expert any version ... output of a single register for StruxureWare ... ... handled by a single register. ... to divide by 10 in such cases ... ... StruxureWare Data Center Expert can be configured ... ... value of either 1 or 2. ... In binary, it would look like this: ... 31000 returns 0000000000000001 If this were a single register, = 1 ... With 2 registers however, you must left shift the 1st register and add it to the second.
Video: Data Center Expert | How do I mass configure APC devices?
... StruxureWare Data Center Expert . ... StruxureWare Data Center Expert (DCE) ... ... StruxureWare Data Center Expert (all versions ... 1 ) Open the Data Center Expert Desktop Client ... can not choose unique settings per device ... It is recommended to ... this with a single device before mass ... 10 ) Change the ... Step 1 : Retrieving configuration ... 1 ) Open the Data Center Expert Desktop Client ... be added to it . 10 ) When finished ... 1 ) Open the Data Center Expert Desktop Client 1 ) Open the Data Center Expert Desktop Client 10 ) Change the ... Step 1 : Retrieving configuration ...
Data Center Expert | Alarm "Device status may be inaccurate due to attempt to transfer DDF failed"
... StruxureWare Data Center Expert message "Device ... ... StruxureWare Data Center Expert (DCE) ... ... StruxureWare Data Center Expert (all versions ... Data Center Expert uses device definition ... ... , Data Center Expert will attempt to ... 1 ) A condition ... causes Data Center Expert to reach out ... ... ) Data Center Expert attempts to connect ... 1 ) Log into the Data Center Expert Desktop Client using ... ... is due to one of the following ... ... for Data Center Expert to retrieve the ... ... within Data Center Expert . 1 ) Log into ... ... , by default it is 21. 1 ) Log into ...


Resultados 1 - 10 de 84

¿No encuentras lo que buscas?

Ponte en contacto con nuestro equipo de atención al cliente para obtener información sobre asistencia técnica, asistencia para quejas, etc.