Consultar las preguntas frecuentes



The Replace Battery indicator light is illuminated on my Conext Battery Backup
... is giving a Replace Battery Indication (Red Replace battery LED w/ ... APC Back-UPS ... ... Test that the battery needs to be replaced soon. ... on and every 14 days following If the Replace Battery indicator is lit ... ... condition of the battery . 3. If the Replace Battery indicator lights again after completing the test, then the battery must be replaced . Contact our customer service for information on replacing your battery . ... Note: The Battery Backup should not be used as a master on off switch. Doing so may cause a premature replace battery LED.
Can I change the individual batteries inside of a Smart-UPS replacement battery cartridge?
APC Replacement Battery Cartridges are intended to be replaced as a complete unit.
Used Battery Disposal Options
If you purchased an APC Replacement Battery Cartridge in the ... to return the old battery will be provided with the new Replacement Battery Cartridge.
Video: Why might my APC Back-UPS Product be beeping?
... is operating on battery power - ... operation to On Battery operation. The Battery Power Supplied outlets are now battery powered. ... entered a low battery condition - ... reached a Low Battery condition and will ... ... only operate on battery for a limited ... ... protect the unit's batteries from discharging too ... With optional APC management software, ... APC's UPS Selector ... -test every 14 days, checking ... integrity of the battery . If the battery fails the self ... the "" Replace Battery "" LED ...
Video: APC AV S Type Power Conditioner w/ Battery Back-up - Battery Replacement Procedure
Environment: UPS is operating Online with a Replace Battery Condition
Why should I use only genuine APC Replacement Battery Cartridge (RBC) in my APC UPS?
Using of a non- APC battery may result in lower runtime, damage the UPS, create hazardous conditions, or void safety certifications ...
Why aren't alarms clearing in the BMS (Battery Management System) AP9921X-AP9922 after replacing batteries?
After changing a battery in a string which is monitored by the APC Battery Management System, it is imperative to clear the old baseline ...
How do I recycle APC batteries in the US and Canada?
Pack the used battery in the packaging from the replacement battery cartridge and affix the return label.
Material Safety Data Sheets (MSDS) or Safety data Sheets (SDS) for Batteries Used in APC UPS Systems
In a few cases, Replacement Battery Cartridges (RBCs) containing High Power Lithium Ion Cell, Phosphate-Based are also used.
Details Returned from APC Devices via Advanced Device Crawlers
Battery Run Time Remaining Battery Replace Indicator


Resultados 1 - 10 de 94

¿No encuentras lo que buscas?

Ponte en contacto con nuestro equipo de atención al cliente para obtener información sobre asistencia técnica, asistencia para quejas, etc.