Consultar las preguntas frecuentes



Data Center Expert | Obtaining an SNMP or Modbus DDF for discovery of third-party devices
... obtain a DDF for StruxureWare Data Center ... to monitor 3rd party devices ? Most APC devices have a Device Definition File ( ... ) within DCE for monitoring device sensors. ... to monitor most third party devices , DCE requires ... ... Association and Searching for Existing DDFs 1 ) Navigate to and search for the Device you would like a DDF for to see if ... already been created for the device . ... you are looking for is displayed in ... ... Requesting a New Device Definition File Installing a Device Definition File within ... Installing a Device Definition File within ... 1 ) Log into ...
Video: Data Center Expert | Device Discovery for Third-Party Devices using SNMP
1 ) You will need to obtain the following information from the device you wish to discover: - snmpv1: Read community string.
Does my APC network enabled device support RADIUS or LDAP?
... APC network enabled device support RADIUS or ... ... APC Network Enabled devices . Refer ... APC Integrated Network Devices can utilize RADIUS ... Dial In User Service ) as a ... These devices include the Network ... ... RFC (Request For Comments) standards for RADIUS authentication. ... All other APC devices do not support ... of authentication except for local device authentication. ... implied fashion, third party tools and software ... ... (LDAP as one possible example) ... ... software server vendor for information on integrating ... ... the APC networked device unless the Service -Type attribute ... Also, ensure that your device is upgraded to the latest firmware version available.
Alert Actions for NetBotz Version 2 and 3 Appliances
Alert Actions for NetBotz Version 2 ... ... via SMTP to one or more target ... via SMTP to one or more target ... message via GSM service provider GPRS / ... Send SNMP V 1 Trap Sends an SNMP version 1 trap to configured ... ... state of an device switch Supported output device such as Output ... Control Pod or third party intelligent power strip ... on an output device Supported output device such as Output ... ... Control Pod or third party intelligent power strip ... speakers Call Web Services Alert Receiver Sends ... via the Web Services API to a ... the NetBotz Web Services API
APC Environmental Sensors FAQ
... be connected to one ap9320 unit? ... are discrete connectors for each APC sensor ... answer is ' one per connector. ... ... 2 female to one male adapter. ... 45 plugs used for in the A ... ... cable, required for proper data transmission ... ... have the following advantages : ( 1 ) more accurate, ... For the relay contacts, what is the accepted current, voltage and resistance? ... 1 A, 30v AC/DC; < 1 ohm ... Can I connect third party sensors to the EMS? ... Yes, any device that allows for relay contacts can be connected to the EMS (two relays are provided).
Data Center Expert | Troubleshooting SNMP Lost Communication to Third Party Devices
... Center Expert and Third - Party devices . Third - Party Devices that support snmpv1 ... APC Devices that use a ... ... communicate with a device . Lost ... and the APC device . ... communication issues to devices . For most APC devices , resolution steps ... know if the device is APC or Third - party , proceed below ... ... Determining if your Device is APC or Third - Party 1 ) Log into ... ... and select the device group in the ... that contains the device in lost communication ... ... click on the device within the Device View pane ( ...
Data Center Expert | How do I update location information for a device?
All third party devices will have a different way of setting the value either via the web interface, console, or possibly through SNMP ...
Video: Data Center Expert | Device Discovery for APC Devices using snmpv1
Discovering APC Devices into Data Center ... APC Devices with NMC supporting ... ... additional knowledge bases for discovering different other types of devices : APC Device : snmpv3 Modbus TCP Devices Third Party devices using SNMP ... discover an snmpv1 Device ... IP Address of device , or subnet device (s) ... ... string (used for APC Device Priority Scanning) ... 1 ) Log into ... ... is an entry for Read and another for Write and that ... ... two entries, one entry with the ... Type will work for both Read ( ...
Data Center Expert | Device Discovery for APC Devices using snmpv3
Discovering APC Devices into Data Center ... APC Devices with NMC supporting ... ... additional knowledge bases for discovering different other types of devices : APC Device : snmpv1 Modbus TCP Devices Third Party devices using SNMP ... discover an snmpv3 Device ... IP Address of device , or subnet device (s) ... 1 ) Log into ... ... Expert can use for communication. ... Host Name fields for the applicable entries ... For a description of ... ... Desktop Client > Device menu > Add Devices . 8) Device Discovery Type > ... ... lead to longer device discovery times. ... number if the device is configured to ...
Video: Data Center Expert | How do I create and manage thresholds?
Custom thresholds need to be created for most third - party devices that are added into DCE.


Resultados 1 - 10 de 86

¿No encuentras lo que buscas?

Ponte en contacto con nuestro equipo de atención al cliente para obtener información sobre asistencia técnica, asistencia para quejas, etc.