Consultar las preguntas frecuentes



Why won't my Lithium-Ion Smart-UPS start when the battery is first connected when there is no utility power to the unit?
... then there will be up to a 1 minute delay between the initial connection of the battery and the UPS being ready to start .
PowerChute Network Shutdown continually shuts down the ESXi host following On Battery Shutdown and UPS turn off when A/C power has been restored in Advanced UPS Configuration.
VMware ESXi versions 4 .x, and 5.x ... Upgrade to PCNS version 4 .x ... 1 . To prevent the ESXi hosts from being continually shut down, re- start the PowerChute Network Shutdown service using the Windows Services console. ... 1 . Issue does not occur for Non-Outlet Aware UPS. ... 4 . Issue does not occur for Single , Redundant or Parallel UPS Configurations.
Can I mix old and new batteries in a Smart-UPS?
... old and new batteries in a Smart ... ... either multiple internal battery cartridges and/ ... to add external batteries . ... old and new battery cartridges within the ... ... Lead Acid) batteries age, their ... ... Smart-UPS batteries are connected in parallel and all batteries are charged at ... Mixing batteries of different ages ... result in some batteries being under charged ... ... and installing the battery cartridges, you should keep the battery cartridges in their ... ... When replacing the batteries in a Smart ... should replace all battery cartridges(internal ... When replacing battery cartridges that are ...
SRT 8 or 10kva experiences excessive battery transfer and re-transfer events in 3 phase systems
excessive battery transfer/retransfer events in 3PH systems. ... 1 . Improved system performance of transitions between Online and Bypass operation modes. 2. Improved system behaviour for three phase input configurations to reduce transitions to battery under certain input feed conditions. ... 4 . Improved system handling for certain AC input conditions during system start -up.
SRT 8 or 10kva reports Error P.11 or DC Bus Soft Start or event codes 124/125
The UPS reports P.11 or DC Bus Soft Start - event 124/125 ... 1 . Improved system performance of transitions between Online and Bypass operation modes. 2. Improved system behaviour for three phase input configurations to reduce transitions to battery under certain input feed conditions. ... 4 . Improved system handling for certain AC input conditions during system start -up.
Why is my UPS emitting a single beep every few mins?
... have observed a single beep being randomly ... ... to the On Battery State (powering ... load from internal batteries ) momentarily and ... Onbattery notification ( 4 beeps every 30 ... ... anomoly and has begun to power the ... from it's internal batteries . If a customer observes their UPS switching to the On Battery State frequently, an adjustment to the UPS thresholds for transfer may be required. ... Note: In one customer's case, we had observed the UPS emitting a single beep, once every 5 mins exactly. Upon removing the internal battery and reconnecting it, the beeping stopped.
How can I adjust the number of battery packs on a Smart-UPS XL?
... how many external batteries are connected so ... ... : Models that begin with SMX are ... can use external batteries . ... and have Smart Batteries . battery packs. battery packs. batteries effects the runtime ... ... is running on battery power. ... number of external batteries . 1 . Using Hyperterminal ... external battery packs ... the number of battery packs via a ... 1 . First , EXIT out ... ... go to: Start |Programs | ... 4 . The port ... data bits, 1 stop bit, ... ... " Adds a battery pack ... number of external battery packs ... " Subtracts a battery pack
Video: How to perform a cold start and brain dead on Smart-UPS
... perform the Cold Start and Brain Dead ... The Cold start procedure is used ... Cold Start : ... use a Cold Start to troubleshoot a bad battery LED as it ... even if the battery is actually bad ... ... is comparing the battery health compared to ... ... attached, the battery will appear healthy ... 1 ) Turn off ... 4 ) UPS should ... end up on battery with 4 beeps every 30 ... ... and function on battery . ... will not cold start , it either ... a functional internal battery . ... perform a Cold Start on a SUA ... 1 ) Turn off ... ... disconnect the internal battery )
What is the proper way to place a single phase Symmetra UPS into maintenance bypass?
... to place a Single -Phase Symmetra ... Single phase Symmetra UPS ... ... state for a single phase Symmetra UPS ... The ideal method of transferring the load to maintenance bypass on a Single -Phase Symmetra UPS is to first command the UPS to bypass before engaging the maintenance bypass switch/breaker. ... 1 . From the PowerView display, go to "Control" / "UPS into Bypass" and press "Return". ... 4 . Now the unit is in Maintenance Bypass. ... Only the Power, Intelligence, and Battery Modules can be safely removed / replaced.
Video: Battery Installation of APC AV Power Conditioners with Battery Back-Up
... and connect the battery in a APC Power Conditioner with Battery Back-Up at first time start -up or following routine battery replacement. ... Power Conditioners with Battery Back-UP Battery must be installed ... ... of-life battery . ... with the internal battery pack disconnected. ... connection of the battery when the front ... ... Connect the internal battery pack as follows ... 1 . Grasp the ... sides (Figure 4 ), and ... ... . Push the Battery Wire Connector ( ... left of the Battery Pack. ... Ensure that the Battery Wire Connector is ...


Resultados 1 - 10 de 98

¿No encuentras lo que buscas?

Ponte en contacto con nuestro equipo de atención al cliente para obtener información sobre asistencia técnica, asistencia para quejas, etc.