Buscar Preguntas Frecuentes
{"searchBar":{"inputPlaceholder":"Busca por palabra clave o haz una pregunta","searchBtn":"Buscar","error":"Ingresa una palabra para buscar"}}
MGE PMM PMN Modbus Register Map
Product line:
MGE PMM/PMN
Environment:
MGE PMM/PMN
Cause:
PMM Facebook Modbus Registers
Resolution:
Below is the Modbus registers for Facebook PMMs and take note that the slave addresses for the breakers change based on the breaker layout. First set of PMM had 4 breakers in panel A and two in panel B. Another set has three breakers in both panels. So labeling will change based on breaker layout.
¿Te fue de ayuda?
Explora más
Explora más