{"searchBar":{"inputPlaceholder":"Busca por palabra clave o haz una pregunta","searchBtn":"Buscar","error":"Ingresa una palabra para buscar"}}
{}

Nuestras marcas

{"support":{"yesButton":"Sí","noButton":"No","feedback":{"title":"¿Qué podemos hacer para mejorar?"},"submitButton":"Enviar","successMessage":"Gracias por tus comentarios","title":"¿Te fue de ayuda?","feedbackPercentLabel":"de las personas encontraron esto útil","captcha":{"error":"Por favor, marca una casilla"}}}
Buscar Preguntas Frecuentes

Video: How to place a Silcon UPS into Maintenance Bypass (MBP)

Issue:
How to place a Silcon UPS in Maintenance Bypass (MBP)
 
Product line:
Silcon
 
Environment:
All Product models, all serial numbers
 
Cause:
This video provides a step by step instruction on how to operate the Silcon UPS into Maintenance Bypass mode, to allow the end-user to power down the UPS without interruption to their load.
 
Resolution:
Press # key
Use the arrow keys to scroll to Bypass Operation: No
Press the C key to change to Bypass Operation: Yes
Press # to store – Display will flash the message "Data Stored"
The Green LED (H003) above Q003 on the bypass panel will illuminate
Turn on Q003
The Green LED (H002) above Q002 on the bypass panel will illuminate
Turn off Q002
 
UPS now in full MBP and the UPS can be shutdown.
 
 

¿No encuentras lo que estás buscando?

Comunícate con nuestro equipo de Atención al Cliente para recibir soporte técnico, asistencia para quejas y más.