Consultar las preguntas frecuentes



How do I update the firmware of my SRT/SMC/XU/XP/SMX/SMT/SCL/SRC/CHS series Smart-UPS using the Firmware Upgrade Wizard?
Issue: ... firmware of the UPS : All Smart - UPS SRT , SMC, ... ... support the below Smart - UPS devices: ... smx1500 with firmware UPS 02.x ... ... These units are 120 V devices built ... ... find your current UPS Firmware version via UPS LCD: ... menu of the UPS LCD screen, ... down to " UPS Firmware". ... find your current UPS Firmware version via ... ... find your current UPS ID: Every Smart - UPS has a unique UPS ID. ... menu on the UPS LCD screen, ... ... same models of UPS have different UPS IDs depending on ...
Video: How do I configure a 208v Smart-UPS RT or SRT for use with a 240v input?
... configure a 208v Smart - UPS RT or SRT for use with ... Smart - UPS Online (RT and SRT ) Smart - UPS RT and SRT units sold in ... The Smart UPS Online line has ... of acceptable input voltages , and as ... ... avoid a sudden voltage shift in the event that the UPS goes to bypass ... to configure the UPS output to match the UPS input. ... turn off the UPS . ... would select the UPS ... . On the UPS tab we would ... The UPS will now output ...
Does my Smart-UPS have Equipment Protection Policy (EPP) coverage?
Does my Smart - UPS have Equipment Protection ... Smart - UPS , Smart - UPS Online ... on many 120v UPS Systems and Surge ... All Smart - UPS and Smart - UPS Online products include ... All 120 volt Line Interactive Smart - UPS offer EPP coverage ... Smart UPS models that do ... All Smart - UPS Online models. ... SURTA, or SRT ... /www. apc .com/ ... ... not your particular UPS features EPP coverage ... If you need to open an EPP claim for your UPS , please contact your local Tech Support Team for assistance.
Video: How do I configure APC Network Management Card network settings?
Return to Top Configuration Method 5 - via Smart - UPS front panel LCD - (Supported SMT, SMX, and SRT
Video: How can I download Event, Data, Configuration, and Debug files from my Network Management Card?
... Enabled products, Smart - UPS Online ( SRT ). ... txt, select UPS debug files ( ... ... txt, select UPS debug files ... X, v 5 .X. ... 5 .) Type ... ... included in the Smart - UPS (su) ... ... Type bye and exit out of your ... 5 .) For the config.ini ... For NMC3: The dbg directory is not included in the Smart - UPS (su) firmware and needs to be manually downloaded. ... apc >logzip ... User (10.10.10.96:(none)): apc
Network Management Card (NMC) Password Reset Procedure
... Enabled products, Smart - UPS Online ( SRT ). ... it with the APC serial configuration cable ... ... a non- APC serial cable during ... ... password on a UPS that has more ... Most UPS devices with a ... ... port at the UPS /Network Management ... Most UPS devices with a ... ... For three phase UPS devices, it ... 5 .) ... password are both apc ... the default, apc ... must repeat step 5 and log on ... ... which are now apc ... serial cable ( APC part number 940 ... 5 .) ... ). Wait 5 -7 ... password are both apc
How can I mass configure a Network Management Card (NMC) or NMC embedded product?
How can I mass configure a Network Management Card (NMC) or NMC embedded product? The five steps below apply ... X and v 5 .X. ... The five steps below apply ... ... and you will exit from the NMC ... ... configuration time. APC by Schneider Electric ... ... .e. Smart - UPS to Smart - UPS , Switched Rack ... ... .e. Smart - UPS to Smart - UPS , Switched Rack ... ... should have ( 5 ) files once ... ... ;SystemUserName= apc ... ;SystemPassword= apc If you leave this character in ... SystemUserName= apc SystemPassword= apc SystemIP=192.168.1. 120 ... 3. Exit ... 3: Exit
Can I mix old and new batteries in a Smart-UPS?
For example, an APC Smart - UPS SRT 5000 system with ... cartridge for the UPS and two battery cartridges for the external battery pack ...
What are the various generations of Smart-UPS Products?
... of single phase Smart - UPS Products? Smart - UPS ... a variety of Smart - UPS products in use ... ... Over the years APC has steadily improved ... ... refer to the apc .com product ... for your specific UPS . Current Products: ... generation Line Interactive Smart - UPS products ... Serial Port on UPS ) Smart -Slot for installation of APC Accessory Cards ... generation Line Interactive Smart - UPS products Voltage adaptability ( 2kva ... ... Serial Port on UPS ) Smart -Slot for installation of APC Accessory Cards ... Level Line Interactive Smart - UPS products ... Serial Port on UPS )
Video: How to perform a cold start and brain dead on Smart-UPS
Smart - UPS ... determine if a UPS is functional if ... ... reset of the Smart - Ups microprocessor. ... establish if a UPS will not turn ... ... and unplug the Smart - UPS from wall. ... front of the UPS until you hear ... 4) UPS should go through ... ... shows that the UPS is functioning correctly ... 5 ) You can now plug your UPS back into the ... ... is acceptable the UPS will transfer back ... If your UPS will not cold ... means that the UPS has suffered an ... Please contact APC Technical support for ... ... a SUA series Smart - UPS :


Resultados 1 - 10 de 64

¿No encuentras lo que buscas?

Ponte en contacto con nuestro equipo de atención al cliente para obtener información sobre asistencia técnica, asistencia para quejas, etc.