Consultar las preguntas frecuentes



Single Phase Symmetra Drops the Load When Returning from Bypass
Input Voltage: Line I 132.7, Line II 132.7, LI-LII 230 VAC Output Voltage Setting: 208 V
Hardwiring to 120v, 208v, and 240v loads from a 208v/240v SmartUPS RT UPS
To supply a 208 v load, the transformer provides: 120 v Hot Leg
Video: How can the Galaxy VS reduce my energy bill?
Galaxy VS is a 20 to 100kva (400v/480v) or 10 to 50kva ( 208v ) 3-phase UPS for edge ...
What are the features of the Galaxy VS NMC 4 based on firmware release?
... /www.se.com/in/ en /download/document/SPD_CCON-BANDZR_ EN /
Galaxy VS; New features, resolved know issues and known issues in firmware release 6.31.3
... /www.se.com/in/ en /download/document/SPD_CCON-BA3KHG_ EN /
What type of battery could I use with the Galaxy VS UPS?
Issue: What kind of external batteries does the Galaxy VS 3-Phase UPS support?
Why can I ping Galaxy VS NMC IP address but cannot access the web page
Issue: Can ping Galaxy VS NMC IP address but cannot access the web page.
Does the NTP need to be configured on all NMCs for all parallel Galaxy VS?
Issue: Does the NTP need to be configured on all NMCs for all parallel Galaxy VS . These includes Internal NCM and optional AP9644 NMC.
Which modular batteries can be used with the Galaxy VS All in One (AIO) model?
Issue: Which modular batteries can be used in the Galaxy VS All in One (AIO) model?
Does the NTP need to be configured on the Galaxy VS internal NMC and the optional AP9644 NMC for all parallel or single Galaxy VS?
Issue: Does the NTP need to be configured on the Galaxy VS internal NMC and the optional AP9644 NMC for all parallel or single Galaxy VS


Resultados 1 - 10 de 52

¿No encuentras lo que buscas?

Ponte en contacto con nuestro equipo de atención al cliente para obtener información sobre asistencia técnica, asistencia para quejas, etc.