Consultar las preguntas frecuentes



50a 208v 3 Phase Rack PDU Load Ratings and Calculations Explained
... 208v 3 Phase Rack PDU Load Ratings ... 3 Phase Rack Power Distribution models ... 50a 3 Phase Rack PDU, such ... ... each bank references two phases: ... Phase 1 and 2 Bank 2 - Phase 2 and 3 ... units where the capacity is limited by ... ... phases 1 and 2 simultaneously. Bank 2 draws current from phases 2 and 3. ... means that phase 2 is supplying current ... banks 1 and 2 . However, ...
Can the ends of a NetShelter 2-post or 4-post rack be closed with panels?
a 4-post rack it creates the look of a cabinet, instead of an open rack .
What is the weight capacity of NetShelter open frame racks: ar201, ar203a and ar204a?
Resolution: ar203a and ar204a Weight Capacity 2 ,000 lb (907.18 kg).
Smart-UPS C Series FAQ
What capacity are the new ... ... 1500va in both Rack and Tower form ... ... Slot and cannot support a Network Management ... SMC rack mount units ship with a rack mount brackets that ... compatible with both 2 and 4 post racks . It can be used ... or threaded hole racks without modification. ... a 4 post rack can purchase a 4 post rack mount rail kit ... 2 years from date of purchase for both the UPS and the Battery ... Press and hold Display button for 2 seconds ... Press and hold the MUTE button, then press the DISPLAY button for 2 seconds
What are some of the applications for the InRow ACRD?
... environments which allows IT managers, facilities ... ... are building new IT assets are looking ... ... great option with its wide range of capacities and ability to ... with loads as it offers the benefits ... ... in this new IT environment by removing ... ... room to adjust capacity . ... modes using a rack inlet temperature probe ... thus protecting expensive IT assets. ~ The InRow RD provides the ability to have two different media of heat rejection both using Direct expansion in addition to its capability of handling low loads of 2 -20kw which makes it a great choice for customers with long term growth plans.
Why is my actual UPS runtime different from the quoted runtime on the APC web page?
... will only reach its optimum capacity after a two or three discharge ... , plus as it ages its capacity will decrease, ... the end of its life.
Rack PDU 2G (AP8XXX) Network Port Sharing Information
Updating firmware for Network Port Sharing Groups If all Rack PDUs in the group ... , simply update the host Rack PDU and it will then update all guest Rack PDUs automatically.
Video: How to mount a Rack Mount Symmetra or Rack Mount Smart-UPS to a 2 Post Rack?
Cause: Some users may be using a 2 post rack instead of a standard 4 post IT Rack .
AP84XX, AP88XX, AP89XX, and AP86XX 2G Rack PDU LCD Backlight Behavior
When should my Rack PDU 2 G LCD remain on and when should it turn off? I have different units displaying different behavior.


Resultados 1 - 10 de 73

¿No encuentras lo que buscas?

Ponte en contacto con nuestro equipo de atención al cliente para obtener información sobre asistencia técnica, asistencia para quejas, etc.