Consultar las preguntas frecuentes



What should I do when encountering an issue with the br1100m2-LM, br1350m2-LM and br1500m2-LM
Schneider Electric has recently identified a non-conforming level of internal operation involving several APC Back-UPS. This non-conformance is limited to the following SKUs;
How accurate are the APC Environmental Monitoring products?
If your horse hoof meter was reading 30%, the Environmental ... read 34.5%, which is about 15-1073744256gh.
Scripting with APC by Schneider Electric Switched Rack Power Distribution Units (PDUs)
Please note: Scripting outlet actions is not available on APC Metered Rack PDUs because they do not offer individual outlet control.
Low output voltage reading on a UPS that uses a step approximated sine wave
When an average responding meter is measuring the stepped approximated output from an APC UPS while operating on battery, this meter will also read ...
Different Types of Voltmeters
When an average responding meter is measuring the stepped approximated output from an APC UPS while operating on battery, this meter will also read ...
Different Types of Voltmeters
When an average responding meter is measuring the stepped approximated output from an APC UPS while operating on battery, this meter will also read ...
Which DHCP options are used when an APC Network Management Device makes a dhcpv4 request?
Devices with an embedded Network Management Card 1 include (but are not limited to): Metered /Switched Rack PDUs (AP78XX, ...
What are the supported port speeds for the APC Network Management Card and network enabled devices?
Devices with an embedded Network Management Card 1 include (but are not limited to): Metered /Switched Rack PDUs (AP78XX, ...


Resultados 1 - 10 de 95

¿No encuentras lo que buscas?

Ponte en contacto con nuestro equipo de atención al cliente para obtener información sobre asistencia técnica, asistencia para quejas, etc.