浏览常见问题解答

Video: Power-Saving Display Mode on Back-UPS XS/RS "G" & "M" Series

发布日期: 18 April 2019

Issue:
Tutorial for toggling the power saving display mode on APC Back-UPS Pro RS/XS/NS G & M models to automatically disable the front display or configure the display for always-on operation.

Product Line:
Back-UPS Pro XS/RS/NS

Environment: 
BR700G/BR1000G/BR1500G
BX850M/BX1000G/BX1300G/BX1350M/BX1500M/BN1080G/BN1350G

Cause:
It may be desired to disable the display when the UPS is in normal operation to avoid visual distraction. Alternately, one may wish to configure the UPS to always illuminate the display for status at-a-glance.

Resolution: 
To toggle the power saver display mode, press and hold the MENU button for 2 seconds until a beep is heard. The default behavior to keep the display active at all times.


对您是否有帮助?

我们如何进行信息改进?

找不到您查找的内容?

请联系我们的客户团队,获取有关技术支持、投诉帮助等的信息。