浏览常见问题解答

Video: Data Center Expert | How do I enable surveillance for NetBotz cameras?

发布日期: 14 July 2020

Issue:
Enabling surveillance in StruxureWare Data Center Expert for NetBotz cameras.

Product Line
StruxureWare Data Center Expert (DCE)
- Basic Appliance (AP9465)
- Standard Appliance (AP9470)
- Enterprise Appliance (AP9475)
- Virtual Appliance (AP94VMACT)
StruxureWare Central (SWC)
InfraStruXure Central (ISXC)
NetBotz v3 Wall Appliance: 355/356 (NBWL0355/6) & 455/456 (NBWL0455/6)
NetBotz v3 Rack Appliance: 450/451 (NBRK0450/1), 550 (NBRK0550), & 570 (NBRK0570)
NetBotz Rack Monitor 750 (NBRK0750)

Environment:
StruxureWare DCE (any version)
NetBotz discovered by DCE (any supported version)

Cause:
This is for customers that require assistance in enabling surveillance for NetBotz cameras in DCE

Resolution:

 
  1. Log into the Data Center Expert client.
  2. Ensure that the NetBotz Appliance with an integrated or attached camera pod is showing within Data Center Expert.  If it has not been discovered yet, reference FA177081.
  3. Each NetBotz camera requires one Surveillance license.  You can verify the licensing that you have installed by going to: System Menu > Server Administration Settings > License Keys.  There will be a specific license type of Surveillance Pack with a total column and a used column.
  4. Select the Surveillance perspective.
  5. Right-click on one of the camera thumbnails and select Surveillance settings. TIP: You can select multiple thumbnails by holding down CTRL or SHIFT and selecting them.
  6. Mark the check box for License Camera.
  7. Enter the Data Center Expert IP address and configure the security options if necessary.
  8. Select the Post Mode that you would like to record the Surveillance clips for.  There are other options to configure if deemed necessary.
  9. Select Apply and OK.

对您是否有帮助?

我们如何进行信息改进?

找不到您查找的内容?

请联系我们的客户团队,获取有关技术支持、投诉帮助等的信息。