浏览常见问题解答

How is the rackmount U-space of a NetShelter cabinet or rack identified?

发布日期: 30 May 2019

Issue: 
Customers need to correctly identify a 'U-space' or 'rack space.'

Product Line: 
NetShelter SX

Environment:
All versions and serial ranges.

Cause: 
Incorrect placement of equipment can create airflow problems, like hot air recirculation.

Resolution: see below


As set forth by the EIA/ECA-310-E Standard:

1. For any Rackmount device or enclosure - a U or unit of rack space is equivalent to 1.75 inches or 44.45 mm.

2. The mounting hole pattern on a rack or enclosure must follow the following guideline:
 
  • Vertical Hole spacing must follow a pattern of 5/8""-5/8""-1/2"" or 15.9mm-15.9mm-12.7mm
  • Horizontal Hole spacing must be 18.3"" or 465 mm (+/- 1.6 mm)
  • Clearance between inner edges of mounting rails must be 450 mm at minimum
  • Outside edges of mounting rail must be 483.4 mm apart at minimum

EIA/ECA-310-E rail specifications in attached file.

To properly mount a device in the rack, a user needs to utilize the notched square mounting hole to indicate the center of a U space. For Example, to mount a 1 U device, 3 mounting holes would be covered by the device with the notched hole residing in the center of the group of 3. Mounting in an "off-U position", effectively moving the installed device 1 hole space up or down is incorrect and will lead to airflow and cooling issues.
 

对您是否有帮助?

我们如何进行信息改进?

找不到您查找的内容?

请联系我们的客户团队,获取有关技术支持、投诉帮助等的信息。