浏览常见问题解答

UPS Performs Continuous Self Tests for One Hour Before Its Scheduled Time

发布日期: 03 June 2014


Issue

A UPS performs continuous self-tests for an hour before it is actually scheduled to perform one.


Product Line

Back-UPS
Smart-UPS
Smart-UPS Online/Smart-UPS RT
Symmetra Power Array
Symmetra RM
Symmetra LX


Environment

PowerChute Plus running on Netware 5 SP 3


Cause

Powerchute Plus 4.3.3 is configured to run a scheduled self test on a Netware 5 SP 3 server. However, the self test begins an hour before the scheduled time and runs continuously for that hour. This issue would only occur on Netware 5 SP 3 servers and only affected those living in states that do not observe Daylight Savings Time, such as Indiana and Arizona. Novell released SP 4 and in their list of "file fixes" it states SP 4" fixed daylight savings time calculations to function properly for time zones where there is no daylight saving and for time zones in the Southern Hemisphere". 


Resolution

Installing SP 4 solves the scheduled self test issue.



对您是否有帮助?

我们如何进行信息改进?

找不到您查找的内容?

请联系我们的客户团队,获取有关技术支持、投诉帮助等的信息。